This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

程序一运行就有BIOS的exception单元报错

Other Parts Discussed in Thread: SYSBIOS

这些打印的错误信息来自BIOSexception单元,程序一开始运行(resume)就出现以下错误提示。有碰到过的人没?

PS:以下错误并非一直存在,是偶尔出现。

SRIO test between DSP and fpga start............................................

SRIO path configuration 4xLaneABCD                     

Link is ok

Running task1 function

Running task1 function

A0=0x17 A1=0x810b29

A2=0x0 A3=0xa

A4=0x810b40 A5=0x0

A6=0x810b29 A7=0x0

A8=0x868888 A9=0x862d6c

A10=0x17 A11=0xc362628

A12=0x810b29 A13=0x1

A14=0x859b8f A15=0xa

A16=0x4 A17=0x867cdc

A18=0x8114b0 A19=0x20

A20=0xc361f7c A21=0x2000020

A22=0x20 A23=0x80002818

A24=0x8000000 A25=0x2820024

A26=0x2000100 A27=0x0

A28=0x4000 A29=0x10

A30=0x0 A31=0x0

B0=0xe B1=0x0

B2=0x0 B3=0x800511a6

B4=0xa B5=0x86c423

B6=0x4 B7=0x86c400

B8=0x8114b8 B9=0xf

B10=0x867eb0 B11=0x80056884

B12=0x0 B13=0x80052cac

B14=0x86c118 B15=0x811344

B16=0x862e38 B17=0x1

B18=0x40 B19=0x80

B20=0x20 B21=0x2a6c800

B22=0x142b2a0 B23=0x100020

B24=0x14120800 B25=0x1000001

B26=0x80025400 B27=0x432c5000

B28=0x0 B29=0x0

B30=0x2900200 B31=0x7f

NTSR=0x10204

ITSR=0xf

IRP=0x8005be7a

SSR=0x0

AMR=0x0

RILC=0x0

ILC=0x0

Exception at 0x8001c8

EFR=0x2 NRP=0x8001c8

Internal exception: IERR=0x9

Instruction fetch exception

Opcode exception

ti.sysbios.family.c64p.Exception: line 248: E_exceptionMin: pc = 0x008001c8, sp = 0x00811344.

To see more exception detail, use ROV or set 'ti.sysbios.family.c64p.Exception.enablePrint = true;'

xdc.runtime.Error.raise: terminating execution