This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

急 C6670 FFTC 驱动问题一个task驱动两个semaphore溢出报错



我想尝试实现在一个task里面驱动两个FFTC同时工作,程序跑固定次数后就报错停止,提示semaphore溢出。所使用的工程是根据andy 提供的keystone的例子工程中的FFTC部分修改的,遇到了前面所述的semaphore溢出的错误。

当程序运行了16384次后,控制台输出如下错误信息:

错误之前FFTC open和flow相关的输出都是在初始化时的输出,使用的是andy提供的例子中的相应的初始化的函数,基本没有修改。

程序运行了16384次后,提示semaphore溢出。

程序中对两个FFTC的配置是完全相同的,没有差别,parse对FFTC完成配置。

我的程序的流程如下(程序在最后):

{

初始化:

FFTC_B分配配置变量空间并配置FFTC_B,

配置rxobj并打开接收流

FFTC_A分配配置变量空间并配置FFTC_A,

配置rxobj_A并打开接收流

中断注册FFTC_B

中断注册FFTC_A

Tx配置(使用FFTC_B)并打开发送流

Tx_A配置(使用FFTC_A)并打开发送流

While(1)

{

         外部调度

         While(pkt)FFTC发送的包的数目,两个FFTC共享

{

         getRequestBuffer(FFTC_B)

         getRequestBuffer(FFTC_A)

         向FFTC_B中的缓存中考入数据

         向FFTC_A中的缓存中考入数据

         发送FFTC_B的请求

         发送FFTC_A的请求

         接收FFTC_B的结果rxGetResult函数

         接收FFTC_A的结果rxGetResult函数

         将FFTC_B的结果拷贝走

         将FFTC_A的结果拷贝走

freeResult  FFTC_B

freeResult  FFTC_B

pkt修改

}

}//end for while(1)

}

下图是我用于观察记录的一些变量

End_time是计算时钟消耗的,其值是TSCL的值作差得到的,timercnt是调度任务的计数器,fftcnt是fft模块的计数器,两个计数器用来统计各个任务的运行次数。

下图是我程序中的semaphore的静态配置,所有semaphore的都在这里。

其中Sem_BCP_2_Schedual暂时没有使用,其他两个semaphore 的Semaphore_post/pend函数都是成对出现的,即觉得这里的semaphore溢出应该不是自己的问题。

我观察了一下semaphore的溢出提示,数字是65535,整好是我的FFTC_task运行次数(16384)的四倍,我的程序中向fftc发送的pkt数目整好也是4个,在想这两个数值之间是否有什么具体的关系?

问题:semaphore的计数器的次数是程序运行次数的4倍,这个怎么理解?错误信息只提供了semaphore溢出作为参考,我应该考虑哪些方向来找到问题所在并修改呢?希望能提供一些debug的思路。还希望各位朋友能给予指点。

以下是我的FFTC_task的主要程序部分:

其中hFFTC_A通过全局变量extern过来的

static Int32 fftc_test_core (Fftc_DrvHandle hFFTC, UInt32 txQNum, Uint8 fftcInstNum)
{
Fftc_RequestHandle hRequestInfo;
Fftc_ResultHandle hResultInfo;
Fftc_TxHandle hTxObj = NULL;
Fftc_RxHandle hRxObj = NULL;
Fftc_TxCfg txCfg;
Fftc_RxCfg rxCfg;
// UInt32 blockExpVal, clipping;
Fftc_BlockInfo blockInfo;
UInt8 *pReqBuffer, *pResultBuffer, *pResultPSInfo, rxFlowId, rxSrcId;
UInt32 maxReqBufferLen, reqBufferLen, resultLen, rxPSInfoLen, txPSInfoLen = 0;
Fftc_Result* pFFTResult = NULL;
Cplx16 *xout, *xoutread;
UInt16 i, j, pktCounter = 0, rxDestnTagInfo;
Int32 retVal;
// UInt32 bIsTestFailed = 0;
FFT_TestCfg* pFFTTestCfg = NULL;
UInt32 blockDataOffset = 0;
UInt32 blockDataOffset_in = 0;
UInt8 coreNum = CSL_chipReadReg (CSL_CHIP_DNUM);

//xm add
Fftc_RequestHandle hRequestInfo_A;
Fftc_ResultHandle hResultInfo_A;
Fftc_TxHandle hTxObj_A = NULL;
Fftc_RxHandle hRxObj_A = NULL;
Fftc_TxCfg txCfg_A;
Fftc_RxCfg rxCfg_A;
FFT_TestCfg* pFFTTestCfg_A = NULL;
Fftc_BlockInfo blockInfo_A;
Int32 retVal_A;
UInt8 *pReqBuffer_A, *pResultBuffer_A, *pResultPSInfo_A, rxFlowId_A, rxSrcId_A;
UInt16 rxDestnTagInfo_A;
Fftc_Result* pFFTResult_A = NULL;
UInt32 maxReqBufferLen_A, reqBufferLen_A, resultLen_A, rxPSInfoLen_A, txPSInfoLen_A = 0;

/* Allocate memory for the test configuration */
if (!(pFFTTestCfg = (FFT_TestCfg *) Fftc_osalMalloc (sizeof (FFT_TestCfg), FALSE)))
{
Fftc_osalLog ("[Core %d]: Error allocating memory for test configuration \n", coreNum);
return -1;
}

/* Read the FFT input vector and configuration for this test
* from the corresponding input configuration file.
* The testCaseId for this test is 6.
*/
if (fftc_parse_testCfg (pFFTTestCfg, &blockInfo) < 0)
{
return -1;
}
/* Setup a Rx flow. This flow will be used to retrieve FFT results
* from a destination queue.
*
* Rx flow Configuration Params:
* -----------------------------
* - Use Host descriptors
* - No PS Info (bPSInfoPresent = 0)
* - Setup Rx object for interrupts + blocking mode
* - Let FFTC driver pick the destination queue (cppiRxQNum = -1)
* - Pick a buffer size big enough to hold the error information and
* FFT result itself.
*/
memset (&rxCfg, 0, sizeof (rxCfg));
rxCfg.useFlowId = -1;
rxCfg.bManageRxFlowCfg = 1;
rxCfg.rxFlowCfg.drvCfg.descType = Cppi_DescType_HOST;
rxCfg.rxFlowCfg.drvCfg.cppiNumDesc = 2;

/* Allocate result buffers big enough to hold:
*
* Per block result = Per block error info (block exp val + clipping detect + srcId + flowId) (16 bytes) +
* block output data (number of samples * sample size)
*/
rxCfg.rxFlowCfg.drvCfg.bufferSize = (pFFTTestCfg->numOutputSamples[0] * FFTC_TEST_SAMPLE_SIZE + 16) * pFFTTestCfg->numBlocks;
rxCfg.rxFlowCfg.drvCfg.bPSInfoPresent = 0;
rxCfg.rxFlowCfg.drvCfg.psLocation = Cppi_PSLoc_PS_IN_DESC;
rxCfg.cppiRxQNum = -1;
rxCfg.bBlockOnResult = 1;
rxCfg.bUseInterrupts = 1;
rxCfg.bManageAccumList = 1; /* Let driver do the Accum Management */
rxCfg.accumCfg.drvCfg.bEnablePacing = 0; /* Disable pacing */
rxCfg.accumCfg.drvCfg.intThreshold = 1; /* Set interrupt threshold to 1 */
Fftc_getDeviceAccumulatorConfig (fftcInstNum, &rxCfg.accumCfg.drvCfg.accChannelNum, &rxCfg.cppiRxQNum);
// Fftc_getDeviceAccumulatorConfig (CSL_FFTC_B, &rxCfg.accumCfg.drvCfg.accChannelNum, &rxCfg.cppiRxQNum);

/* Get a Rx Object Handle */
if ((hRxObj = Fftc_rxOpen (hFFTC, &rxCfg)) == NULL)
{
Fftc_osalLog ("[Core %d]: Rx flow open failed \n", coreNum);
goto error;
}
else
{
Fftc_osalLog ("[Core %d]: Rx Flow %d opened successfully using Rx queue %d \n", coreNum,
Fftc_rxGetFlowId (hRxObj), Fftc_rxGetRxQueueNumber (hRxObj));
}

//xm add
/* Allocate memory for the test configuration */
if (!(pFFTTestCfg_A = (FFT_TestCfg *) Fftc_osalMalloc (sizeof (FFT_TestCfg), FALSE)))
{
Fftc_osalLog ("[Core %d]: Error allocating memory for test configuration FFTC instance 1\n", coreNum);
return -1;
}

/* Read the FFT input vector and configuration for this test
* from the corresponding input configuration file.
* The testCaseId for this test is 6.
*/
if (fftc_parse_testCfg (pFFTTestCfg_A, &blockInfo_A) < 0)
{
return -1;
}
/* Setup a Rx flow. This flow will be used to retrieve FFT results
* from a destination queue.
*
* Rx flow Configuration Params:
* -----------------------------
* - Use Host descriptors
* - No PS Info (bPSInfoPresent = 0)
* - Setup Rx object for interrupts + blocking mode
* - Let FFTC driver pick the destination queue (cppiRxQNum = -1)
* - Pick a buffer size big enough to hold the error information and
* FFT result itself.
*/
memset (&rxCfg_A, 0, sizeof (rxCfg_A));
rxCfg_A.useFlowId = -1;
rxCfg_A.bManageRxFlowCfg = 1;
rxCfg_A.rxFlowCfg.drvCfg.descType = Cppi_DescType_HOST;
rxCfg_A.rxFlowCfg.drvCfg.cppiNumDesc = 2;

/* Allocate result buffers big enough to hold:
*
* Per block result = Per block error info (block exp val + clipping detect + srcId + flowId) (16 bytes) +
* block output data (number of samples * sample size)
*/
rxCfg_A.rxFlowCfg.drvCfg.bufferSize = (pFFTTestCfg_A->numOutputSamples[0] * FFTC_TEST_SAMPLE_SIZE + 16) * pFFTTestCfg_A->numBlocks;
rxCfg_A.rxFlowCfg.drvCfg.bPSInfoPresent = 0;
rxCfg_A.rxFlowCfg.drvCfg.psLocation = Cppi_PSLoc_PS_IN_DESC;
rxCfg_A.cppiRxQNum = -1;
rxCfg_A.bBlockOnResult = 1;
rxCfg_A.bUseInterrupts = 1;
rxCfg_A.bManageAccumList = 1; /* Let driver do the Accum Management */
rxCfg_A.accumCfg.drvCfg.bEnablePacing = 0; /* Disable pacing */
rxCfg_A.accumCfg.drvCfg.intThreshold = 1; /* Set interrupt threshold to 1 */
Fftc_getDeviceAccumulatorConfig (0, &rxCfg_A.accumCfg.drvCfg.accChannelNum, &rxCfg_A.cppiRxQNum);
// Fftc_getDeviceAccumulatorConfig (CSL_FFTC_B, &rxCfg.accumCfg.drvCfg.accChannelNum, &rxCfg.cppiRxQNum);

/* Get a Rx Object Handle */
if ((hRxObj_A = Fftc_rxOpen (hFFTC_A, &rxCfg_A)) == NULL)
{
Fftc_osalLog ("[Core %d]: FFTC 0 Rx flow open failed \n", coreNum);
goto error;
}
else
{
Fftc_osalLog ("[Core %d]: FFTC 0 Rx Flow %d opened successfully using Rx queue %d \n", coreNum,
Fftc_rxGetFlowId (hRxObj_A), Fftc_rxGetRxQueueNumber (hRxObj_A));
}

// register_rx_interrupts (CSL_FFTC_A,hRxObj);
register_rx_interrupts_fftc (fftcInstNum, hRxObj);

//xm register fftc_a
register_rx_interrupts_fftc (0, hRxObj_A);

/* Setup a Tx Object. This object will be used to submit FFT requests.
*
* Tx object Configuration Params:
* -----------------------------
* - Pre-alloc Tx Free Desc (bManageReqBuffers = 1)
* - Use Host descriptors
* - Pick a buffer size big enough to hold all the
* FFT request blocks.
* - No PS Info (bPSInfoPresent = 0)
* - No mixed size DFTs (bEnableDftSizeListCfg = 0)
* - Open queue in shared mode (bSharedMode = 1).
* Enables re-programming queue using CPPI.
*/
memset (&txCfg, 0, sizeof (txCfg));
txCfg.txQNum = (Fftc_QueueId) txQNum;
txCfg.bManageReqBuffers = 1;
txCfg.bEnableDftSizeListCfg = 0;
txCfg.fftQCfg = pFFTTestCfg->fftcQCfg;
txCfg.bSharedMode = 1;
txCfg.descType = Cppi_DescType_HOST;
txCfg.cppiNumDesc = 2;
txCfg.bufferSize = pFFTTestCfg->numInputSamples[0] * FFTC_TEST_SAMPLE_SIZE * pFFTTestCfg->numBlocks;
txCfg.bPSInfoPresent = 0;

/* Get a Tx Object Handle */
if ((hTxObj = Fftc_txOpen (hFFTC, &txCfg)) == NULL)
{
Fftc_osalLog ("[Core %d]: Tx open failed \n", coreNum);
goto error;
}


//xm add
/* Setup a Tx Object. This object will be used to submit FFT requests.
*
* Tx object Configuration Params:
* -----------------------------
* - Pre-alloc Tx Free Desc (bManageReqBuffers = 1)
* - Use Host descriptors
* - Pick a buffer size big enough to hold all the
* FFT request blocks.
* - No PS Info (bPSInfoPresent = 0)
* - No mixed size DFTs (bEnableDftSizeListCfg = 0)
* - Open queue in shared mode (bSharedMode = 1).
* Enables re-programming queue using CPPI.
*/
memset (&txCfg_A, 0, sizeof (txCfg));
txCfg_A.txQNum = (Fftc_QueueId) txQNum;
txCfg_A.bManageReqBuffers = 1;
txCfg_A.bEnableDftSizeListCfg = 0;
txCfg_A.fftQCfg = pFFTTestCfg_A->fftcQCfg;
txCfg_A.bSharedMode = 1;
txCfg_A.descType = Cppi_DescType_HOST;
txCfg_A.cppiNumDesc = 2;
txCfg_A.bufferSize = pFFTTestCfg_A->numInputSamples[0] * FFTC_TEST_SAMPLE_SIZE * pFFTTestCfg_A->numBlocks;
txCfg_A.bPSInfoPresent = 0;

/* Get a Tx Object Handle */
if ((hTxObj_A = Fftc_txOpen (hFFTC_A, &txCfg_A)) == NULL)
{
Fftc_osalLog ("[Core %d]: FFTC 0 Tx open failed \n", coreNum);
goto error;
}

// int count =0;

int pingpong = 0;
//由于循环CP添加必须是4的倍数 而引起的多余循环CP的数位 最后需要去除掉
int CP_more = 0;
//实际需要的CP
int PrefixAddNum = 0;

while(1)
{
Semaphore_pend(Sem_re_2_fftc, BIOS_WAIT_FOREVER);
fftcnt++;
start_time = TSCL;

pingpong = (pingpong+1)%2;
pktCounter = 0;
OutputDataOffset = 0;
OutputDataOffset_A = 0;
blockDataOffset_in = 0;
// if(count %30 ==0)
// OutputDataOffset = 4416*2;

//xm 做4次FFT,分别为1+6+1+6
/*
*这里天线端口数应该和pktConter相关,天线端口数乘以2为pktCounter的值
*因为一个task驱动了两个FFTC,两个共同配合完成FFT的计算
*此处的修改需要在后面继续完善!!!!!!!!!!
*包括端口号与pktCounter的对应关系,以及CPmode的影响
*/
/* Run the test in a loop */
while (pktCounter != 4)//NUM_TEST_PACKETS)
{
/* No PS info */
txPSInfoLen = 0;

/* Initialize the request buffer offset */
blockDataOffset = 0;
// blockDataOffset_in = 0;

if((pktCounter%2)==0)
{
// Get the number of FFT blocks
pFFTTestCfg->numBlocks = 1;
PrefixAddNum = PrefixAddNum_A;
pFFTTestCfg->fftcQCfg.cyclicPrefixRegConfig.cyclicPrefixAddNum = ((PrefixAddNum_A+3)>>2)*4;

//xm add
pFFTTestCfg_A->numBlocks = 1;
PrefixAddNum = PrefixAddNum_A;
pFFTTestCfg_A->fftcQCfg.cyclicPrefixRegConfig.cyclicPrefixAddNum = ((PrefixAddNum_A+3)>>2)*4;
}
else
{
// Get the number of FFT blocks
pFFTTestCfg->numBlocks = 6;
PrefixAddNum = PrefixAddNum_B;
pFFTTestCfg->fftcQCfg.cyclicPrefixRegConfig.cyclicPrefixAddNum = ((PrefixAddNum_B+3)>>2)*4;

//xm add
pFFTTestCfg_A->numBlocks = 6;
PrefixAddNum = PrefixAddNum_B;
pFFTTestCfg_A->fftcQCfg.cyclicPrefixRegConfig.cyclicPrefixAddNum = ((PrefixAddNum_B+3)>>2)*4;
}

/* Get the input and output data info for each of the blocks now */
for (i = 0; i < pFFTTestCfg->numBlocks; i ++)
{
/* Account for zero pad samples too. */
pFFTTestCfg->numOutputSamples[i] = pFFTTestCfg->numInputSamples[i];
if (pFFTTestCfg->fftcQCfg.controlRegConfig.bZeroPadEnable)
pFFTTestCfg->numOutputSamples[i] += pFFTTestCfg->fftcQCfg.controlRegConfig.zeroPadFactor;
if (pFFTTestCfg->fftcQCfg.cyclicPrefixRegConfig.bCyclicPrefixAddEnable)
pFFTTestCfg->numOutputSamples[i] += pFFTTestCfg->fftcQCfg.cyclicPrefixRegConfig.cyclicPrefixAddNum;

//xm add
/* Account for zero pad samples too. */
pFFTTestCfg_A->numOutputSamples[i] = pFFTTestCfg_A->numInputSamples[i];
if (pFFTTestCfg_A->fftcQCfg.controlRegConfig.bZeroPadEnable)
pFFTTestCfg_A->numOutputSamples[i] += pFFTTestCfg_A->fftcQCfg.controlRegConfig.zeroPadFactor;
if (pFFTTestCfg_A->fftcQCfg.cyclicPrefixRegConfig.bCyclicPrefixAddEnable)
pFFTTestCfg_A->numOutputSamples[i] += pFFTTestCfg_A->fftcQCfg.cyclicPrefixRegConfig.cyclicPrefixAddNum;
}

/* Get a request buffer */
if (Fftc_txGetRequestBuffer (hTxObj,
&blockInfo,
&pFFTTestCfg->fftcQCfg,
txPSInfoLen,
Fftc_rxGetFlowId (hRxObj),
pktCounter,
&hRequestInfo,
&pReqBuffer,
&maxReqBufferLen) < 0)
{
Fftc_osalLog ("[Core %d]: Unable to get request buffer \n", coreNum);
goto error;
}

//xm add
/* Get a request buffer */
if (Fftc_txGetRequestBuffer (hTxObj_A,
&blockInfo_A,
&pFFTTestCfg_A->fftcQCfg,
txPSInfoLen,
Fftc_rxGetFlowId (hRxObj_A),
pktCounter,
&hRequestInfo_A,
&pReqBuffer_A,
&maxReqBufferLen_A) < 0)
{
Fftc_osalLog ("[Core %d]: FFTC 0 Unable to get request buffer \n", coreNum);
goto error;
}

/* Initialize the whole FFT request buffer */
memset (pReqBuffer, 0, maxReqBufferLen);

//xm add
memset (pReqBuffer_A,0,maxReqBufferLen_A);

/* The request buffer MUST be populated in the following order:
*
* <PS Info to be passed to receiver> then followed by <FFT request data>
*/
/* We have no Protocol Specific Pass through data to pass to receiver in this test.
* So just copy the FFT request data itself into the request buffer, block by block
*/
//xm 这个两个的长度是一样的
reqBufferLen = pFFTTestCfg->numBlocks * pFFTTestCfg->numInputSamples[0] * FFTC_TEST_SAMPLE_SIZE;
for (i = 0; i < pFFTTestCfg->numBlocks; i ++)
{
// Copy the FFT request block A
memcpy ((Ptr) (pReqBuffer + blockDataOffset),//头头对其,所以间隔0byte
(Ptr) (0x0C1DF300+blockDataOffset_in),//RE后的首地址
RE_number*2);
// Fftc_osalLog ("Iput BLocK address:%x \n", (Uint32)(void *)(0x0C1812C0+ inputDataOffset) );
// Copy the FFT request block B
memcpy ((Ptr) (pReqBuffer + blockDataOffset+RE_number*2+4),//前面A的600*=2400,和中间子载波补0,所以间隔2404byte
(Ptr) (0x0C1DF300+RE_number*2+blockDataOffset_in),//B是RE后的首地址加上(RE个数的一半*4)
RE_number*2);
// Fftc_osalLog ("Iput BLocK address:%x \n", (Uint32)(void *)(0x0C1812C0+ inputDataOffset) );

//xm add
memcpy ((Ptr) (pReqBuffer_A + blockDataOffset),//头头对其,所以间隔0byte
(Ptr) (0x0C1EF980+blockDataOffset_in),//RE后的首地址
RE_number*2);
memcpy ((Ptr) (pReqBuffer_A + blockDataOffset+RE_number*2+4),//前面A的600*=2400,和中间子载波补0,所以间隔2404byte
(Ptr) (0x0C1EF980+RE_number*2+blockDataOffset_in),//B是RE后的首地址加上(RE个数的一半*4)
RE_number*2);

//xm 两组数据完全一样,不再做区分
blockDataOffset_in += (4800);//由于输入数组就是按照1200的格式排列的,所以这里的4800在任何带宽下都不变
blockDataOffset += (pFFTTestCfg->numInputSamples[0] * FFTC_TEST_SAMPLE_SIZE);//根据不同带宽而改变
}

#ifdef FFTC_TEST_DEBUG
Fftc_osalLog ("\n[Core %d]: Submitting FFT Request ... \n", coreNum);
#endif

/* Submit the FFT request for processing */
if (Fftc_txSubmitRequest (hTxObj,
hRequestInfo,
reqBufferLen) < 0)
{
Fftc_osalLog ("[Core %d]: Unable to submit request \n", coreNum);
goto error;
}
else
{
#ifdef FFTC_TEST_DEBUG
Fftc_osalLog ("Submitted request %d successfully \n", pktCounter);
#endif
}

//xm add
/* Submit the FFT request for processing */
if (Fftc_txSubmitRequest (hTxObj_A,
hRequestInfo_A,
reqBufferLen) < 0)
{
Fftc_osalLog ("[Core %d]: FFTC 0 Unable to submit request \n", coreNum);
goto error;
}
else
{
#ifdef FFTC_TEST_DEBUG
Fftc_osalLog ("FFTC 0 Submitted request %d successfully \n", pktCounter);
#endif
}

/* -------------------------------------
* Wait on FFT result and verify Result
* -------------------------------------
*/
#ifdef FFTC_TEST_DEBUG
Fftc_osalLog ("\n[Core %d]: Waiting for Result ... \n", coreNum);
#endif

/* Get the raw result from the engine. */
if ((retVal = Fftc_rxGetResult (hRxObj,
&hResultInfo,
&pResultBuffer,
&resultLen,
&pResultPSInfo,
&rxPSInfoLen,
&rxFlowId,
&rxSrcId,
&rxDestnTagInfo
)) != FFTC_RETVAL_SUCCESS)
{
Fftc_osalLog ("[Core %d]: Invalid FFT result : %d \n", coreNum, retVal);
goto error;
}

//xm add
/* Get the raw result from the engine. */
if ((retVal_A = Fftc_rxGetResult (hRxObj_A,
&hResultInfo_A,
&pResultBuffer_A,
&resultLen_A,
&pResultPSInfo_A,
&rxPSInfoLen_A,
&rxFlowId_A,
&rxSrcId_A,
&rxDestnTagInfo_A
)) != FFTC_RETVAL_SUCCESS)
{
Fftc_osalLog ("[Core %d]: FFTC 0 Invalid FFT result : %d \n", coreNum, retVal_A);
goto error;
}
// else
// {
// Fftc_osalLog("[Core %d]: FFTC 0 valid FFT result: %d \n",coreNum,retVal_A);
// }

CP_more = (((PrefixAddNum+3)>>2)*4 -PrefixAddNum)*4;//乘4是因为4byte一个RE

if(CP_more != 0)
{
for (i = 0; i < pFFTTestCfg->numBlocks; i ++)
{
// memcpy((void*)(g_aucsrioBuf+OutputDataOffset+PrefixAddNum+i*(FFTsize+PrefixAddNum)), (void*)(pResultBuffer+CP_more), (FFTsize)*4);
// CP_more += (FFTsize);

memcpy((void*)(g_aucsrioBuf+OutputDataOffset+i*(FFTsize+PrefixAddNum)), (void*)(pResultBuffer+CP_more), (FFTsize+PrefixAddNum)*4);
CP_more += (FFTsize + ((PrefixAddNum+3)>>2)*4)*4;
}
OutputDataOffset = (OutputDataOffset+pFFTTestCfg->numBlocks*(FFTsize+PrefixAddNum));

// CACHE_wbL1d ((void *)g_aucsrioBuf, SRIO_SEND_BUF_MAX_LEN*4, CACHE_WAIT);
// _mfence();
}
else
{
//edma参数设置 挺简单的
vusr_edma_wr_setup_all_payload((Uint32)(pResultBuffer), (Uint32)(void *)(g_aucsrioBuf+OutputDataOffset), resultLen, 8+pktCounter);
// Fftc_osalLog ("BLocK address:%x \n", (Uint32)(void *)(g_aucsrioBuf + OutputDataOffset) );

//edma触发
verify_edma_complete(8+pktCounter);

OutputDataOffset = (OutputDataOffset+resultLen/4);
}

//xm add
CP_more = (((PrefixAddNum+3)>>2)*4 -PrefixAddNum)*4;//乘4是因为4byte一个RE

if(CP_more != 0)
{
for (i = 0; i < pFFTTestCfg_A->numBlocks; i ++)
{
// memcpy((void*)(g_aucsrioBuf+OutputDataOffset+PrefixAddNum+i*(FFTsize+PrefixAddNum)), (void*)(pResultBuffer+CP_more), (FFTsize)*4);
// CP_more += (FFTsize);

memcpy((void*)(g_aucsrioBuf +30720 +OutputDataOffset_A+i*(FFTsize+PrefixAddNum)), (void*)(pResultBuffer_A+CP_more), (FFTsize+PrefixAddNum)*4);
CP_more += (FFTsize + ((PrefixAddNum+3)>>2)*4)*4;
}
OutputDataOffset_A = (OutputDataOffset_A+pFFTTestCfg_A->numBlocks*(FFTsize+PrefixAddNum));

// CACHE_wbL1d ((void *)g_aucsrioBuf, SRIO_SEND_BUF_MAX_LEN*4, CACHE_WAIT);
// _mfence();
}
else
{
//edma参数设置 挺简单的
vusr_edma_wr_setup_all_payload((Uint32)(pResultBuffer_A), (Uint32)(void *)(g_aucsrioBuf +30720 +OutputDataOffset_A), resultLen_A, 12+pktCounter);
// Fftc_osalLog ("BLocK address:%x \n", (Uint32)(void *)(g_aucsrioBuf + OutputDataOffset) );

//edma触发
verify_edma_complete(12+pktCounter);

OutputDataOffset_A = (OutputDataOffset_A+resultLen_A/4);
}

/* Done using the result buffer, return it to the FFTC driver for recycling */
if (Fftc_rxFreeResult (hRxObj,
hResultInfo
) < 0)
{
Fftc_osalLog ("[Core %d]: Error freeing result : %d \n", coreNum, i);
goto error;
}

//xm add
if (Fftc_rxFreeResult (hRxObj_A,
hResultInfo_A
) < 0)
{
Fftc_osalLog ("[Core %d]: FFTC 0 Error freeing result : %d \n", coreNum, i);
goto error;
}

pktCounter ++;

//delete xm 暂不使用srio传输
/* 这部分SRIO的传输可能会带来一定时延,目前需要一个方法来解决*/
if(pktCounter == 2)
{
// complete = 0;
// Srio_SendData((Uint32*)SRC_BASE, (Uint32*)(DST_BASE1), SLOT_SIZE, DEV1_ID);//每次发一个port的端口
// while(complete == 0);
}
else if(pktCounter == 4)
{
// complete = 0;
// Srio_SendData((Uint32*)(SRC_BASE+SLOT_SIZE*1), (Uint32*)(DST_BASE1+SLOT_SIZE*1), SLOT_SIZE, DEV1_ID);
// while(complete == 0);

}
else if(pktCounter == 6)
{
// complete = 0;
// Srio_SendData((Uint32*)(SRC_BASE+SLOT_SIZE*2), (Uint32*)(DST_BASE2), SLOT_SIZE, DEV1_ID);
// while(complete == 0);
}

}

// complete = 0;
// Srio_SendData((Uint32*)(SRC_BASE+SLOT_SIZE*3), (Uint32*)(DST_BASE2+SLOT_SIZE*1), SLOT_SIZE, DEV1_ID);
// while(complete == 0);
// Srio_SendDoorbell(DEV0_INFO, DEV1_ID);

end_time = TSCL - start_time;
// printf("FFTC time used is %d\n",end_time);

// 做完CP166 8次
// Semaphore_post(Sem_BCP_2_Schedual);
}

/* Free the FFT input, output data and test configuration memory allocated */
fftc_clean_testCfg (pFFTTestCfg, &blockInfo);

/* Close all FFTC handles */
if (hRxObj)
Fftc_rxClose (hRxObj);

if (hTxObj)
Fftc_txClose (hTxObj);

//xm add
/* Free the FFT input, output data and test configuration memory allocated */
fftc_clean_testCfg (pFFTTestCfg_A, &blockInfo_A);

/* Close all FFTC handles */
if (hRxObj_A)
Fftc_rxClose (hRxObj_A);

if (hTxObj_A)
Fftc_txClose (hTxObj_A);

/* Return success. */
return 0;

error:
/* Free the FFT result info memory */
if (pFFTResult)
Fftc_osalFree (pFFTResult, sizeof (Fftc_Result), FALSE);

/* Free the FFT input, output data and test configuration memory allocated */
fftc_clean_testCfg (pFFTTestCfg, &blockInfo);

/* Close all FFTC handles */
if (hRxObj)
Fftc_rxClose (hRxObj);

if (hTxObj)
Fftc_txClose (hTxObj);

//xm add
/* Free the FFT result info memory */
if (pFFTResult_A)
Fftc_osalFree (pFFTResult_A, sizeof (Fftc_Result), FALSE);

/* Free the FFT input, output data and test configuration memory allocated */
fftc_clean_testCfg (pFFTTestCfg_A, &blockInfo_A);

/* Close all FFTC handles */
if (hRxObj_A)
Fftc_rxClose (hRxObj_A);

if (hTxObj_A)
Fftc_txClose (hTxObj_A);

/* Return error */
return -1;
}

  • 补充提问:

    在FFTC的例程里有用函数Fftc_allocFreeqBuffers中使用memalloc为每个bolck分配了数据的存储空间,其中memalloc的第一个参数heap给的是NULL,在SYS/BIOS的帮助中说如果这个参数给的值是NULL,则在默认的heap中分配空间,我在工程的cfg中文件中使用如下语句配置了一个heap

    var heapMemParams1 = new HeapMem.Params;
    heapMemParams1.size = 8192*60;
    heapMemParams1.sectionName = "systemHeap";
    Program.global.heap0 = HeapMem.create(heapMemParams1);

    这里在memalloc时,变量是在这个“systemHeap”里面进行分配的吧?(对这部分一直不是很理解)

  • 再补充一个问题:

    下面这段错误还是这个程序出现的。此时在程序一开始运行时在while(1)的semaphore后打一个断点,当程序进来后去掉断点,然后让程序一直运行一段时间,此时,系统没有提示如最开始提问的那样semaphore溢出的错误,但当再次在while(1)后面打一个断点时,系统就会输出这样的错误,我此时并不能判断是否是我的程序的错误。第一个问题说到的运行到固定次数的semaphore溢出的错误时在程序一开始就在while(1)里有一个断点,带断点运行几次后,去掉断点再连续运行时出现的。

    请问这又是什么原因造成的?

    Trouble Setting Breakpoint with the Action "Remain Halted" at 0x8a9968:
    (Error -1202 @ 0x8A997C)
    Device core is hung. The debugger will attempt to force the device to a ready state to recover debug control. Your application's state will be corrupt. You should have limited access to memory and registers, but you may need to reset the device to debug further.
    (Emulation package 5.0.872.0)