看了DM8168的datasheet,发现DM8168的HDMI好像没有RX,只有TX。而DM8168的Dome板的资料又说DM8168的HDMI有RX功能,想了解DM8168是有还是没有RX功能,如果没有RX,Dome有这个功能是怎么实现的。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
看了DM8168的datasheet,发现DM8168的HDMI好像没有RX,只有TX。而DM8168的Dome板的资料又说DM8168的HDMI有RX功能,想了解DM8168是有还是没有RX功能,如果没有RX,Dome有这个功能是怎么实现的。
Hi ,
芯片上集成了HDMI TX. HDMI RX 是需要外置芯片来扩展的。
你找一下比如Silicon Image的网站上搜搜
DM8168的功耗觉得有点大,请问下还没有类似的产品可以替代:参数要求,a、1个USB口;b、2个PHY(集成或者提供接口都可以);c、提供1600*1200的分辨率;d、可接收DVI信号,同时接收DVI信号后做264的压缩,以23帧左右的速率存入SATA硬盘内(200G-500G)。
对DM8168的开发难度大想更换方案,目前考虑DM388和DMVA3,先考虑DM388不行在考虑DMVA3.
1、DM388的问题是不知道DM388的PCI可以接SATA硬盘不?从资料上看,写的是DM388的PCI是做从。
2、想问DM388和DMVA3有没有公司在使用?
3、DM388和DMVA3的功耗怎样?
1. 可以做host也就是RC的。外接PCI-e to SATA桥片没问题。
2. of course...
3. 看你具体跑的东西了。低功耗模式下1080p30,在参考设计上可以做到整机4w不到
想问下如果用DM388或者DMVA3,同时处理H.264的压缩、视频的存储(存入1T的SATA硬盘)和视频输出(通过PHY),只考虑芯片的角度,DM388或DMVA3会不会出现卡顿的情况?
DM38x手册上没有SATA口。
从带宽上是没有问题的。你这个是很典型的单路编码器应用。