Part Number: TDA4VM
使用官方提供的systool将底层的pinmux重新整理了一遍,在系统中目前是可以找到所有的GPIO了

但是当我在MCU1_0中启用了csl库的gpio初始化函数,函数如下
#define PWM_IN1_PORT 1
#define PWM_IN1_PIN 13
#define PWM_IN1_CFG 0
#define PWM_IN2_PORT 1
#define PWM_IN2_PIN 14
#define PWM_IN2_CFG 1
#define PWM_IN3_PORT 1
#define PWM_IN3_PIN 11
#define PWM_IN3_CFG 2
#define PWM_IN4_PORT 0
#define PWM_IN4_PIN 60
#define PWM_IN4_CFG 3
GPIO_PinConfig MygpioPinConfigs[] =
{
/* Input pin with interrupt enabled */
GPIO_DEVICE_CONFIG(PWM_IN1_PORT, PWM_IN1_PIN) | GPIO_CFG_IN_INT_RISING | GPIO_CFG_INPUT,
GPIO_DEVICE_CONFIG(PWM_IN2_PORT, PWM_IN2_PIN) | GPIO_CFG_IN_INT_RISING | GPIO_CFG_INPUT,
GPIO_DEVICE_CONFIG(PWM_IN3_PORT, PWM_IN3_PIN) | GPIO_CFG_IN_INT_RISING | GPIO_CFG_INPUT,
GPIO_DEVICE_CONFIG(PWM_IN4_PORT, PWM_IN4_PIN) | GPIO_CFG_IN_INT_RISING | GPIO_CFG_INPUT,
};
GPIO_CallbackFxn MygpioCallbackFunctions[] =
{
NULL,
NULL,
NULL,
NULL,
};
void Cap_init()
{
uint8_t bank_num = 0;
GPIO_v0_HwAttrs gpio_cfg1;
GPIO_v0_HwAttrs gpio_cfg2;
GPIO_v0_HwAttrs gpio_cfg3;
GPIO_v0_HwAttrs gpio_cfg4;
GPIO_socGetInitCfg(PWM_IN4_PORT, &gpio_cfg4);
gpio_cfg4.baseAddr = CSL_WKUP_GPIO0_BASE;
// bank_num = PWM_IN4_PIN/16;
// gpio_cfg4.intCfg[PWM_IN4_PIN].intNum = CSLR_GPIOMUX_INTRTR0_IN_GPIO0_GPIO_BANK_0 + bank_num;
// gpio_cfg4.intCfg[PWM_IN4_PIN].intcMuxNum = INVALID_INTC_MUX_NUM;
// gpio_cfg4.intCfg[PWM_IN4_PIN].intcMuxInEvent = 0;
// gpio_cfg4.intCfg[PWM_IN4_PIN].intcMuxOutEvent = 0;
GPIO_configIntRouter(PWM_IN4_PORT, PWM_IN4_PIN, 0, &gpio_cfg4);
GPIO_socSetInitCfg(PWM_IN4_PORT, &gpio_cfg4);
GPIO_socGetInitCfg(PWM_IN1_PORT, &gpio_cfg1);
gpio_cfg1.baseAddr = CSL_GPIO1_BASE;
// gpio_cfg1.intCfg[PWM_IN1_PIN].intNum = CSLR_GPIOMUX_INTRTR0_IN_GPIO0_GPIO_BANK_0 + bank_num;
// gpio_cfg1.intCfg[PWM_IN1_PIN].intcMuxNum = INVALID_INTC_MUX_NUM;
// gpio_cfg1.intCfg[PWM_IN1_PIN].intcMuxInEvent = 0;
// gpio_cfg1.intCfg[PWM_IN1_PIN].intcMuxOutEvent = 0;
GPIO_configIntRouter(PWM_IN1_PORT, PWM_IN1_PIN, 0, &gpio_cfg1);
GPIO_socSetInitCfg(PWM_IN1_PORT, &gpio_cfg1);
GPIO_socGetInitCfg(PWM_IN2_PORT, &gpio_cfg2);
gpio_cfg2.baseAddr = CSL_GPIO1_BASE;
GPIO_configIntRouter(PWM_IN2_PORT, PWM_IN2_PIN, 0, &gpio_cfg2);
GPIO_socSetInitCfg(PWM_IN2_PORT, &gpio_cfg2);
GPIO_socGetInitCfg(PWM_IN3_PORT, &gpio_cfg3);
gpio_cfg3.baseAddr = CSL_GPIO1_BASE;
GPIO_configIntRouter(PWM_IN3_PORT, PWM_IN3_PIN, 0, &gpio_cfg3);
GPIO_socSetInitCfg(PWM_IN3_PORT, &gpio_cfg3);
GPIO_v0_config.pinConfigs = MygpioPinConfigs;
GPIO_v0_config.callbacks = MygpioCallbackFunctions;
GPIO_v0_config.numberOfPinConfigs = sizeof(MygpioPinConfigs) / sizeof(GPIO_PinConfig);
GPIO_v0_config.numberOfCallbacks = sizeof(MygpioCallbackFunctions) / sizeof(GPIO_CallbackFxn);
GPIO_v0_config.intPriority = 0x8;
GPIO_init();
GPIO_setCallback(PWM_IN1_CFG, PwmInCap1Callback);
GPIO_enableInt(PWM_IN1_CFG);
GPIO_setCallback(PWM_IN2_CFG, PwmInCap2Callback);
GPIO_enableInt(PWM_IN2_CFG);
GPIO_setCallback(PWM_IN3_CFG, PwmInCap3Callback);
GPIO_enableInt(PWM_IN3_CFG);
GPIO_setCallback(PWM_IN4_CFG, PwmInCap4Callback);
GPIO_enableInt(PWM_IN4_CFG);
}
linux的设备树如下(节选):
&wkup_gpio0 {
pinctrl-names = "default";
pinctrl-0 = <&wakegpio0_pins_default>;
};
&main_gpio0 {
pinctrl-names = "default";
pinctrl-0 = <&mygpio0_pins_default>;
};
&main_gpio1 {
pinctrl-names = "default";
pinctrl-0 = <&mygpio1_pins_default>;
};
当包含着上述的系统在启动时,其日志会打印报错:
[ 3.805209] davinci_gpio 42110000.gpio: IRQ index 3 not found [ 3.810951] davinci_gpio 42110000.gpio: error -ENXIO: IRQ not populated [ 3.821153] davinci_gpio 601000.gpio: IRQ index 0 not found [ 3.826738] davinci_gpio 601000.gpio: error -ENXIO: IRQ not populated
启动后,就找不到wakeup和GPIO1的控制端口了;
我不太理解Cls gpio库的初始化函数怎么会与davinci_gpio的驱动函数起冲突,请问有没有人能解释下问题?其实调用CLS库也是为做GPIO中断,我怀疑是在找寻中断号的过程中起了冲突,如果是这样请问该如何解决呢?