This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求各位大神推荐一款带有1394接口的嵌入式开发板



解释说明一下:本人最近在做一个项目,通过下位机来控制显微镜的自动对焦,通过摄像头拍摄到的数据传输给下位机DSP处理。因此其中出现一个接口问题就是现在的开发板基本上没有1394接口。而且显微镜卖方提供的摄像头大多都是1394接口的。因此要想在下位机上实现显微镜自动对焦的话就比较困难。现在有几个问题如下:

                1、想找一款具有1394接口的DSP开发板,最好是也能够集成ARM核

                 2、如果找不到具有1394接口的开发板,我现在有一款OMAPL138,那么我想问问大家谁能给我一份基于linux的USB摄像头驱动。这个驱动太难搞定了。但是由于1394的传输帧率比USB的要快,这样如果选用USB 的话在效率上可能会受到影响。

                 3、有没有谁知道如果说利用USB转1394接口的话,这样的驱动能不能找得着。

最后先感谢大家百忙之中与我讨论,或者有什么更好的方案!