This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP4470 H.264编解码评估问题



我们评估了OMAP4470的H.264编解码,有些疑问需要核实一下,另外我们发现的一些现象描述和分析如下,请确认或更正。

1、 通过阅读代码,我们注意到IVAHD的频率是可调的,且最高可设到500MHz,且通过修改代码改变IVAHD的频率可以提高或者降低H.264编解码的运行速率。

2、 当IVAHD频率设置到500MHz时,单独H.264 High Profile编码一帧的耗时经多次测试平均耗时均在16ms一下,也就是可以达到60FPS。

3、 IVAHD可以长期稳定工作在500MHz的频率上么?能够保证长期稳定工作的IVAHD频率是多少?想长期稳定工作在500MHz需要采取什么措施?