我有一个4096*720的视频需要264编码,分成4路1024*720给到4个DM365,怎样做到编码器的同步?
也就是说,对于同一帧4096*720的图像,4个DM365对分到的1024*720的图像采取的把它都是作为I帧,或者都是P帧来编码,不会出现一路是I帧码流,另一路是P帧
在使用码率控制的情况下,看手册说可能会产生丢帧,一旦发生了丢帧,4路编码器就可能对接下来的图像采用不同的编码方式,可以通过关闭码率控制,使用固定的帧内、帧间量化参数QP,做到编码时不丢帧,每编码完一帧就即时的读出这一帧的码流吗?