This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678 SGMII link up = 0问题



各位专家,大家好

这里有一个问题,很多人也提过,还有些不明白。按照6678开发板设计的板子,也是采用的88E1111作为PHY芯片,使用SGMII1,电源时钟以及内存测试均正常。

1、插上网线上电之后,网口的LED_LINK1000指示灯常亮,LED_RX对应的指示灯会闪烁。

2、测试使用GE测试程序,MAC、SGMII、SERDES三种环路内部测试均正常。

3、对板子进行初始化,使用platform.c里面的platform_init(),程序会运行到Init_SGMII(1)的时候,读取sgmiiStatus的值,发现bIsLinkUp的值为0,也就是link up失败。从上面看来,DSP的MAC、SGMII和SERDES是不是没有什么问题啊,能够确定是PHY的问题吗?

还有,使用GE的进行DSP0_TO_DSP1模式的测试的时候,具体应该怎么操作呢,有详细的测试文档吗,谢谢!!!