This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAPL138 WatchDog Reset疑问

Other Parts Discussed in Thread: OMAP-L138

spruh77a.pdf 《OMAP-L138 DSP+ARM Processor Technical Reference Manual》文档中31.2.2 Architecture – Watchdog Timer Mode提到

This section describes the use of the timer as a watchdog timer. In order to fully function in watchdogtimer mode, the timer must be internally connected to the device hardware reset signal. 

31.2.2.1 Watchdog Timer中又提到这样的内容:
When the timeout event occurs, the watchdog timer resets the entire processor.

31.1.2 Features中提到这样的内容:

Generates interrupts to CPU
• Generates sync events to DMA
• Generates output event to device reset (watchdog only)
• Generates output event to timer output pins (if pins are available)
• External event capture via timer input pins (if pins are available)


So,综合上面的内容理解,WatchDog发生超时时产生硬件复位是自动完成的,且不需要外部连接(TM64P_OUT12)到CPU硬件复位引脚?如果是这样,

今天我按文档要求配置WatchDog后,查看Watchdog Timer Control Register (WDTCR)寄存器,Bit15 WDFLAG标记已经发生超时,但是CPU并没有发生复位。

麻烦哪位使用过的朋友,帮忙解释一下?