This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于C6678 EVM板与PC机通过网口通信的问题

我在尝试C6678的EVM板与电脑通过网口进行通信。我用的是TI提供的工程,其路径是ti/mcsdk-2-00-04-16/examples/ndk/helloworld/evmc6678l。我改动的地方是hello.c中的

char * LocalIPAddr = "192.168.1.120";
char * LocalIPMask = "255.255.255.0";
char * GateWayIP = "0.0.0.0.";
其他地方都没有改动。我电脑的IP地址是192.168.1.124.
运行程序后,Console窗口中提示:
Timeout waiting for reply from PA to pa_addrMac command
Add_MAC Address Failed.
Error: Unable to register the EMAC.
NIMUIOCTL Failed with error code :-22.
Service Status : DHCPC :Failed :000
总是提示MAC地址没有加上,传送数据也不成功。
请问,TI提供的这个工程还有哪些地方需要改动吗?或者是还需要什么设置?C6678与电脑通过网口通信的具体操作步骤是怎样的呢?有没有针对这个工程的一些使用说明之类的?
期待各位高手指点,不胜感激!