This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

am3354 gpmc和FPGA通信的问题

Other Parts Discussed in Thread: AM3354

 最近在写一个am3354和FPGA通信的Linux驱动, FPGA是16位,异步,不复用引脚设备,使用的片选2,下面是我的驱动程序,无法实现两者的数据传输,跪求指教!

#include <linux/kernel.h> #include <linux/platform_device.h> #include <linux/gpio.h> #include <linux/delay.h> #include <linux/interrupt.h> #include <linux/io.h> #include <linux/module.h> #include <linux/slab.h> #include <linux/init.h> #include <linux/fs.h> #include <linux/delay.h> #include <plat/board.h> #include <plat/gpmc.h> #include <plat/gpmc-smc91x.h> #include <asm/uaccess.h> #include <linux/dma-mapping.h> #include <linux/string.h>

static int major ; static struct class *gpmc_fpga_cls; static struct device *gpmc_fpga_dev; static char __iomem *fpga_access_base; dma_addr_t fpga_phy_base;

#define GPCM_FPGA_CS              2            //FPGA选择通道3 #define FPGA_ACCESS_SIZE          SZ_16M//FPGA通道的大小

static struct gpmc_timings fpga_default_timings = {

 .sync_clk = 0,

 .cs_on = 0,  .cs_rd_off = 89,  .cs_wr_off = 57,

 .adv_on = 3,  .adv_rd_off = 9,  .adv_wr_off = 9,

 .we_on  = 3,  .we_off = 48,    .oe_off = 89,

 .access = 80,  .rd_cycle = 96,  .wr_cycle = 57,

}; static void gpmc_write_reg(int idx, u32 val) {  writel(val, gpmc->io_base + idx); }

static u32 gpmc_read_reg(int idx) {  return readl(gpmc->io_base + idx); }

static int gpmc_fpga_open(struct inode * inode, struct file * file) {  unsigned long val;

 /*申请GPMC通道*/     if(gpmc_cs_request(GPCM_FPGA_CS,FPGA_ACCESS_SIZE,&fpga_phy_base) < 0)     {      printk("fail to gpmc_cs_request!\n");   return -1;     }

 if (!request_mem_region(fpga_phy_base, FPGA_ACCESS_SIZE,     "gpmc_fpga_mem"))  {   printk("fail to request_mem_region\n");   return -EBUSY;  }  else   printk("fpga_phy_base = 0x%0x\n",fpga_phy_base);    fpga_access_base = ioremap(fpga_phy_base,FPGA_ACCESS_SIZE);    if(fpga_access_base == NULL)  {   printk("fail to ioremap!\n");   return -ENOMEM;  }    gpmc_write_reg(GPMC_IRQENABLE, 0);  gpmc_write_reg(GPMC_TIMEOUT_CONTROL, 0);    /*3,利用内核提供的函数设置时序*/  gpmc_cs_set_timings(GPCM_FPGA_CS,&fpga_default_timings);    return 0; } static ssize_t gpmc_fpga_read(struct file *flle, char __user *ubuf, size_t count, loff_t *ppos) {  int ret = 0;  unsigned int temp;

 temp = readl(fpga_access_base + 0x31);  if(copy_to_user(ubuf,&temp ,count))   {    ret = -EINVAL;   }

 return ret; }

static ssize_t gpmc_fpga_write(struct file *file, const char __user *ubuf, size_t count, loff_t *ppos) {  int ret = 0;  unsigned int temp;

 if(copy_from_user(&temp ,ubuf ,count))   ret = -EINVAL;  else   {    writel(temp,fpga_access_base + 0x31);    *ppos += count;    ret = count;   }

 return ret; }

static struct file_operations  gpmc_fpga_fops = {  .open  = gpmc_fpga_open,  .read  = gpmc_fpga_read,  .write = gpmc_fpga_write,  .owner = THIS_MODULE, };

static int gpmc_fpga_init(void) {  int val;  printk("gpmc_fpga_init\n");  major = register_chrdev(0, "gpmc_fpga", &gpmc_fpga_fops);  gpmc_fpga_cls = class_create(THIS_MODULE, "gpmc_fpga");  gpmc_fpga_dev = device_create(gpmc_fpga_cls, NULL, MKDEV(major, 0), NULL, "gpmc_fpga_dev"); /* /dev/buttons */

 return 0; }

static void gpmc_fpga_exit(void) {  iounmap(fpga_access_base);  gpmc_cs_free(GPCM_FPGA_CS);  device_destroy(gpmc_fpga_cls,MKDEV(major, 0));  class_destroy(gpmc_fpga_cls);  unregister_chrdev(major,"gpmc_fpga");    return ; }

module_init(gpmc_fpga_init); module_exit(gpmc_fpga_exit); MODULE_LICENSE("GPL");