Getting Started With the AM17x EVM里的
Installing the SDK software一节中有如下表述:
The PSP package is available as part of the SDK AM1x_arm_#_#_#_#.tar.gz installation in the
DaVinci-PSP-SDK-#.#.#.# directory under the main installation directory. Issue following command for un-taring
the installer:
host$ tar -xvzf AM18x_1_10_#_#.tar.gz
可是DaVinci-PSP-SDK-#.#.#.# 里并没有host$ tar -xvzf AM18x_1_10_#_#.tar.gz。
多谢!