我需要用到RPU单元里的告诉GPO,号称PRU里面的GPO能达到100M的翻转速率,但我从来没用过,请问基本的控制步骤是什么,有什么例程可以参考吗?就是用一个PRU的IO产生一个50Mhz的方波,急求解决方法,谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你们有查过自己代码的汇编实现吗?还是说就是用的c编译器。如果只是用c的编译器的话,建议看下生成的汇编。一个指令周期5ns,所以要想高速的话,还是要看看需要几条汇编指令能实现你想要的翻转。
我是直接用C语言实现的,gcc交叉编译的,我想知道的是,这个I/O翻转速度是因为自己编程的原因无法提升,还是说翻转速度只能达到这样
是通过R30寄存器控制的PRU专用I/O吗?
控制普通的GPIO达不到这个速度。
谢谢您啦!普通I/O口最高只有2M左右,AM3352好像并没有PRU