This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

c6655 sgmii MAC层互联



大家好 老师你们好

     有一问题请教一下,我有一个客户用C6655,一个系统上用了10个,每个板卡有一个C6655,这样总共有10个C6655,每块板子通过网络将数据传给CPU,

我们选择博通的一款SGMII SWITCH芯片,请教一下,C6655 SGMII 可以直接连接到博通交换芯片的SGMII上吗,这种方式可以省掉很多千兆PHY芯片以及网络变压器,极大降低班子尺寸和成本