This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM62A: am62a的SDK编译问题

Part Number: PROCESSOR-SDK-AM62A


我根据TI的文档,编SDK的时候出现了问题:
配置文件是processor-sdk-analytics-09_02_00-config;
包是ti-processor-sdk-linux-edgeai-am62axx-evm-09_02_00_05-Linux-x86-Install.bin;
虚拟机配置如下:
执行以下命令编译SDK
./oe-layertool-setup.sh -f configs/processor-sdk-analytics/processor-sdk-analytics-<version>-config.txt
cd build
. conf/setenv
echo 'ARAGO_BRAND = "edgeai"' >> conf/local.conf
MACHINE="am62axx-evm" bitbake -k tisdk-edgeai-image
编译结果:可以看到有五个任务出错。
于是,我重新编译,再次执行命令:
MACHINE="am62axx-evm" bitbake -k tisdk-edgeai-image
它一直在do_fetch下载ti-tidl-AUTOINC+default-r0_edgeai_2这个资源,耗费大量时间。。。

我的问题是:
1、为什么上述五个任务没有编译通过呢?要怎么看是哪里的问题?
2、为什么每次我重新编译,都会去下载ti-tidl-AUTOINC+default-r0_edgeai_2这个资源,不应该是下到本地的吗?然后根据本地文件是否存在这个依赖库,如果没有再去repo。
3、我的ubuntu的ram够吗?会不会是ram问题导致编译失败。
4、这个工程大概耗费我300多G,这是正常现象吗?