我用8168的SCLR的SC3做缩放遇到性能问题(同时缩放多路1080p视频)。
如果我开2个SCLR的link来缩放,性能是否就会提高一倍?
还有dvr_rdk4.0默认只有2个SCLR的link,我是否可以增加SCLR的个数?
DM8168中一共有5个scalar,我过缩放的输入、输出都是420sp的,是否只能用SC3和SC4来缩放?
SCLR这link是否只能用SC3,SC5来缩放。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我用8168的SCLR的SC3做缩放遇到性能问题(同时缩放多路1080p视频)。
如果我开2个SCLR的link来缩放,性能是否就会提高一倍?
还有dvr_rdk4.0默认只有2个SCLR的link,我是否可以增加SCLR的个数?
DM8168中一共有5个scalar,我过缩放的输入、输出都是420sp的,是否只能用SC3和SC4来缩放?
SCLR这link是否只能用SC3,SC5来缩放。
你好;
1、请查看hdvpss性能手册:
DVRRDK_04.00.00.03/ti_tools/hdvpss/dvr_rdk_hdvpss/docs/HDVPSS_FeaturePerformanceGuide.pdf
2、单个sclr性能 "about 230-240 MP/s (mega pixels/sec) in TI816x",
如果开2个sclr理论上可以提升一倍,具体看程序
3、sclr 在程序中只能使用sc3 和sc5
4、缩放,你可以在测试一下sc1,和sc2;
有通过swms调用的时候输出是yuv420,这个你可以实测一下
谢谢Ternence Hsu 的解答。另外还有个问题,DVRRDK4默认只有2个sclr 的link,我是否可以通过修改代码将sclr 增加到4个或者更多个呢?
我建立了2个sclr,都用的SC3来缩放,发现性能并没有增加。
如果是1个sclr缩放,缩放一帧1080p数据平均要8.5ms;如果2个sclr缩放,那么缩放一帧1080p数据平均要17ms。
是我参数没设置对,还是建多个sclr对并不会提示性能。