我们是通过FPGA做的视频采集,实现1HD(1080P60 or 1080P30) + 4SD,FPGA和8168通信使用GPMC总线, 1080P原始数据每帧3~4Mb,。请问GPMC的极限速度能达到多少呢?还是FPGA能实现部分压缩?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我们是通过FPGA做的视频采集,实现1HD(1080P60 or 1080P30) + 4SD,FPGA和8168通信使用GPMC总线, 1080P原始数据每帧3~4Mb,。请问GPMC的极限速度能达到多少呢?还是FPGA能实现部分压缩?
1080p的原始数据每帧这个尺寸做不到吧?是Byte吧。
建议用PCI-E或者VIN口来传。
嗯 犯二了 . 是byte。 原始数据1080P是不是要求GB/s以上才行呢
像你这种情况,建议
1. PCI-E实现DM8168和FPGA通信, 或者
2. FPGA 采集后,连接到DM8168的VIN口,使用BT1120协议传图像。
你好,
1. 如果是PCIE, FPGA就会采集到自己的内存再传入8168的DDR?
2. VIN的话,芯片直接输出到VIN接口,直接传输到M3下的SR?