This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8148的TVP5158驱动

Other Parts Discussed in Thread: TVP5158

最近在调试基于DM8148的tvp5158驱动,但是有几个奇怪的问题迷惑着我。

1、为什么官方的内核里面没有TVP5158的驱动?驱动要如何获得?网上找不到基于8148的5158驱动。

2、ti_tools里面有一个hdvpss的工具,理解应该和M3有关系,但是是独立编译的,好像和dvr_rdk编译的时候没关联,这个是做什么用的?

3、内核里面有一个vpss的驱动,这个又是干什么的,和上面有没有关系?

  • 你用的是DVRRDK吗?里面有带TVP5158的配置的。

  • 是的,配置我已经找到了,谢谢!不过还有一个疑问,DM8148的数据手册描述支持8路D1,但是我分析dvrrdk发现好像最高只能支持到8路half-D1, 请问数据手册上面说的是8路D1是full-D1还是half-D1,谢谢!

  • 8路D1应该是可以的。你从哪里分析得到不能支持?

    在DM8168上甚至支持16-D1

  • 你好,我还没有硬件,只试验了四路的,我是从hdvpss软件里面的头文件看到的,如下

    /* Multi channel standards from here Please add all VESA standards enums
           above this only. this is to ensure proxy Oses compatibility */
        FVID2_STD_MUX_2CH_D1 = 0x200,
        /**< Interlaced, 2Ch D1, NTSC or PAL. */
        FVID2_STD_MUX_2CH_HALF_D1,
        /**< Interlaced, 2ch half D1, NTSC or PAL. */
        FVID2_STD_MUX_2CH_CIF,
        /**< Interlaced, 2ch CIF, NTSC or PAL. */
        FVID2_STD_MUX_4CH_D1,
        /**< Interlaced, 4Ch D1, NTSC or PAL. */
        FVID2_STD_MUX_4CH_CIF,
        /**< Interlaced, 4Ch CIF, NTSC or PAL. */
        FVID2_STD_MUX_4CH_HALF_D1,
        /**< Interlaced, 4Ch Half-D1, NTSC or PAL. */
        FVID2_STD_MUX_8CH_CIF,
        /**< Interlaced, 8Ch CIF, NTSC or PAL. */
        FVID2_STD_MUX_8CH_HALF_D1,
        /**< Interlaced, 8Ch Half-D1, NTSC or PAL. */

     头文件里面列出来支持的通道数和格式,最下面的就是8路的half-d1;

  • TVP5158 支持一种叫做 cascade级联的模式。你说的8-half D1 就是说可以两片 TVP5158 直接相连,而只用其中一片TVP5158的BT656口和主芯片传递图像。

    这种级联模式适合VP口资源不多的主芯片。而DM8148上面可以直接接多达4个TVP5158, 所以是不需要考虑用级联的这种方式的。

  • 你好,我也在做DM8148的板子,我也想试验四路的,但对这方面不太解,可不可以指导一下,谢谢~

  • DVRRDK里面已经支持了TVP5158 接入4D1的用例。使用的是一个8位口。

  • 8位口是怎么回事,我不了解,从来没跑过4D的demo,不知道怎么将它跑起来,望指导一下,非常感谢~  可以QQ联系我,我QQ是1363017608

  • yzhang6_10 说:

    8位口是怎么回事,我不了解,从来没跑过4D的demo,不知道怎么将它跑起来,望指导一下,非常感谢~  可以QQ联系我,我QQ是1363017608

    你好;

           不知道你是用的什么版本的SDK;

            如果是用的DVRRDK,可以参考dvr_rdk/mcfw/src_linux/mcfw_api/usecases/ 目录下面的usecase来进行参考设计;

           如usecase : multich_progressive_4d1_vcap_venc_vdec_vdis.c

  • 4d1的usecase需要从一个8位的口接入4路视频信号吗?如果只接入一路视频信号,usecase能正常执行吗?