This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP C 6416 HPI 数据总线 写 冲突

Other Parts Discussed in Thread: TMS320C6416

芯片型号:TMS320C6416  -600MHz

现象:用CPU的本地总线 通过HPI对 DSP进行读写操作——可以正确读,不能写入

1、用示波器测量:

a、当总线上某个数据位写入1,DSP相应寄存器的 对应数据位值为“0”,则测量到的值为 0.8V;

b、当总线上某个数据位写入1,DSP相应寄存器的 对应数据位值为“1”,则测量到的值为 3.3V;

c、当总线上某个数据位写入0,DSP相应寄存器的 对应数据位值为“1”,则测量到的值为 2.1V;

d、当总线上某个数据位写入0,DSP相应寄存器的 对应数据位值为“0”,则测量到的值为 0V;

2、外围电路配置与我司某设计相同,只是CPU更换了。

??? 该问题与什么相关? 总线时序?