This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368视频监控项目-----OSD及实时视频缩放功能异常请帮忙指点!!

1、项目背景:

         我们的项目,参考了DM368_EVM的设计,基于DVSDK_V4.02开发软件,要在DM368上实现:

         PAL视频实时输入输出、实时h.264视频编解码、实时视频缩放、实时视频(含标签)本地存储、硬件OSD叠加UI。

 

   2、困难描述:

         2.1 实时视频缩放功能异常:

           2.1.1 移植video_loopback_resize异常:

                dmai_2_20_00_15的video_loopback_resize不支持365/368。

                配置CONFIG_DM368_IPIPE, 参考video_loopback_dm368.cfg和video_loopback_resize_dm355.cfg

                移植video_loopback_resize_dm368.cfg后,生成video_loopback_resize_dm368.x470MV,但是,运行

                出现多种异常,如“ davinci_resizer: mode doesn't allow multiple instances: 2"等。

           2.1.2 capture_prev_rsz_onthe_fly_yuv只能缩小(降采样):

               用的是 linux-driver-examples-psp03.01.01.38/imp-prev-rsz中的例程。

               只能缩小(降采样),若放大,就出现蓝屏。       

           2.1.3 困惑:

                a)  DM368应该有实时PAL制视频缩放成功的案例吗?

                b)capture_prev_rsz_onthe_fly_yuv只能缩小,是否说明“davinci_resizer"驱动能工作?

                c)  参考video_loopback_dm368.cfg和video_loopback_resize_dm355.cfg

                     移植video_loopback_resize_dm368.cfg,没有发现要修改的配置。

                d) 进一步调试,从如何下手?请指点。

 

         2.2  OSD异常:

               2.2.1  OSD驱动例程异常:

                         linux-driver-example中的osd例程blend等,控制台能输出OSD1的属性,视频输出口只显示白屏。

                        <image001.png>

               2.1.3 困惑:

                         怎么能确定OSD驱动是否能正常工作?怎么有什么注意事项?