This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352 Linux系统下NandFlash GPMC资源分配问题



各位TI大牛:

     Linux系统下 NandFlash GPMC资源是如何分配的呢?片选这个不说了,直接明了,起始地址?地址范围呢?

我查看了下源代码,没有找到明确的设置地方,跟踪了下内核启动信息,添加打印,看到了如下结果

gpmc ncs0 nand flash:startaddr 8000000 memory size 1000000

起始地址128M 大小16M

程序里面是怎么设定的呢?

am335x_nand_init (board_am335xevm.c)调用     board_nand_init()(board-flash.c)

void
161 __init board_nand_init(struct mtd_partition *nand_parts,
162             u8 nr_parts, u8 cs, int nand_type)
163 {  
164     board_nand_data.cs      = cs;
165     board_nand_data.parts       = nand_parts;
166     board_nand_data.nr_parts    = nr_parts;
167     board_nand_data.devsize     = nand_type;
168
169     board_nand_data.ecc_opt = OMAP_ECC_HAMMING_CODE_DEFAULT;
170     board_nand_data.gpmc_irq = OMAP_GPMC_IRQ_BASE + cs;
171
172     if (cpu_is_am335x()) {
173 //      board_nand_data.ecc_opt  = OMAP_ECC_BCH8_CODE_HW;
174         board_nand_data.xfer_type = NAND_OMAP_PREFETCH_POLLED;
175     }
176
177     gpmc_nand_init(&board_nand_data);
178 }

这里设置了片选,分区信息

board_nand_data.devsize     = nand_type;//怎么理解,devsize设备大小?nandtype nand类型,看程序nand_type = 0x00,不解、、

再后面就是调用gpmc_nand_init进行底层初始化了。

int __init gpmc_nand_init(struct omap_nand_platform_data *gpmc_nand_data)
 85 {
 86     int err = 0;
 87     struct device *dev = &gpmc_nand_device.dev;
 88
 89     gpmc_nand_device.dev.platform_data = gpmc_nand_data;
 90
 91     err = gpmc_cs_request(gpmc_nand_data->cs, NAND_IO_SIZE,
 92                 &gpmc_nand_data->phys_base);
 93     if (err < 0) {
 94         dev_err(dev, "Cannot request GPMC CS\n");
 95         return err;
 96     }
 97
 98      /* Set timings in GPMC */
 99     err = omap2_nand_gpmc_retime(gpmc_nand_data);
100     if (err < 0) {
101         dev_err(dev, "Unable to set gpmc timings: %d\n", err);
102         return err;
103     }
104
105     /* Enable RD PIN Monitoring Reg */
106     if (gpmc_nand_data->dev_ready) {
107         gpmc_cs_configure(gpmc_nand_data->cs, GPMC_CONFIG_RDY_BSY, 1);
108     }
109
110     err = platform_device_register(&gpmc_nand_device);
111     if (err < 0) {
112         dev_err(dev, "Unable to register NAND device\n");
113         goto out_free_cs;
114     }
115
116     return 0;
117
118 out_free_cs:
119     gpmc_cs_free(gpmc_nand_data->cs);
120
121     return err;
122 }

 NAND_IO_SIZE   4

gpmc_cs_request(gpmc_nand_data->cs, NAND_IO_SIZE,  &gpmc_nand_data->phys_base);

片选申请  这个NAND_IO_SIZE 又是什么含义?

int gpmc_cs_request(int cs, unsigned long size, unsigned long *base)
403 {
404     struct resource *res = &gpmc_cs_mem[cs];
405     int r = -1;
406
407     if (cs > GPMC_CS_NUM)
408         return -ENODEV;
409
410     size = gpmc_mem_align(size);
411     if (size > (1 << GPMC_SECTION_SHIFT))
412         return -ENOMEM;
413
414     spin_lock(&gpmc_mem_lock);
415     if (gpmc_cs_reserved(cs)) {
416         r = -EBUSY;
417         goto out;
418     }
419     if (gpmc_cs_mem_enabled(cs))
420         r = adjust_resource(res, res->start & ~(size - 1), size);
421     if (r < 0)
422         r = allocate_resource(&gpmc_mem_root, res, size, 0, ~0,
423                       size, NULL, NULL);
424     if (r < 0)
425         goto out;
426    
427     gpmc_cs_enable_mem(cs, res->start, resource_size(res));
428     printk("gpmc ncs0 nand flash:startaddr %x memory size %x\n",res->start,resource_size(res));
429     *base = res->start;
430     gpmc_cs_set_reserved(cs, 1);
431 out:
432     spin_unlock(&gpmc_mem_lock);
433     return r;
434 }

gpmc_cs_request 又是如何得出 128M起始地址 16M大小的呢?

请高手指点?