This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352外部存储器接口咨询

Other Parts Discussed in Thread: AM3352

各位好,想请教一个AM3352外部存储器的问题,如果我想采用地址和数据总线分离(不复用)的方式,并且同时支持512K×16bit(19根地址线)的NOR FLASH和64K×16(16根地址线)的SRAM访问,地址总线接口该如何定义?程序从NOR FLASH启动;FLASH采用CSn0,SRAM采用CSn1。请问AM335x是否支持这种设计?

对比参考手册第7章和第26章的表格7-5和26-9,在address和dadabus不复用模式下,这两章的表格对于外部16bit NOR FLASH的地址总线接口定义不一致,在设计过程中到底是参考哪一章的内容呢?