This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ccs5.1编译出错



各位专家,在CCS5.1中,我利用File-New-Ccs project建立了一个新的工程,工程选择为Empty project。在main.c里面输入如下代码:

#include <c6x.h>

#include <stdio.h>

#include <ti/csl/csl_chip.h>

void main(void) {

uint32_t coreID = CSL_chipReadReg (CSL_CHIP_DNUM);

return;

}

为什么Build工程时会出现错误。如下:

error #10234-D: unresolved symbols remain

error #10010: errors encountered during linking; "lk.out" not built。是不是在工程设置的地方需要设置一下?

谢谢大家解答。

  • 您好,

    需要在properties->CCS build->C6000 linker->file search path中添加csl lib,如"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\csl\lib\ti.csl.ae66"

    另外请注意以后在发帖时将问题全部贴上,不要只贴一部分,这样方便解答,谢谢

  • ANDY 你好,

    在这个文件夹下有很多类似的文件,比如还有ti.csl.ae66.mk,请问在建立工程时,我该怎么选择那一个文件呢?是不是只要用到了CSL函数就必须按照您说的方法添加csl lib?谢谢。

  • ANDY 你好,

    为什么6678开发板的例子SRIO_LoopbackDioIsrexampleproject的File search path没有CSL lib,工程的设置如下

    我在论坛里下载的工程文件IPC_example_on_6678,在File Search Path中除了添加\ti.csl.ae66,还需要添加什么文件吗?因为添加ti.csl.ae66后build工程后出现错误如下

    Description Resource Path Location Type
    #10010 errors encountered during linking; "IPC_example_on_6678.out" not IPC_example_on_6678    C/C++ Problem
    <a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML/10234.html">#10234-D</a>  unresolved symbols remain IPC_example_on_6678    C/C++ Problem
    unresolved symbol CSL_intcGlobalEnable, first referenced in ./ipc_interrupt.obj IPC_example_on_6678    C/C++ Problem
    unresolved symbol CSL_intcGlobalNmiEnable, first referenced in ./ipc_interrupt.obj IPC_example_on_6678    C/C++ Problem
    unresolved symbol CSL_intcHwControl, first referenced in ./ipc_interrupt.obj IPC_example_on_6678    C/C++ Problem
    unresolved symbol CSL_intcInit, first referenced in ./ipc_interrupt.obj IPC_example_on_6678    C/C++ Problem
    unresolved symbol CSL_intcOpen, first referenced in ./ipc_interrupt.obj IPC_example_on_6678    C/C++ Problem
    unresolved symbol CSL_intcPlugEventHandler, first referenced in ./ipc_interrupt.obj IPC_example_on_6678    C/C++ Problem
    谢谢。

     

  • 您好!

    1. ti.csl.ae66.mk 是makefile文件,添加ti.csl.ae66即可

    2. 再 添加 ti.csl.intc.ae66,注意路径的设置

  • 你好,请问有没有文件或者链接,说明什么情况下需要添加 ti.csl.intc.ae66,或者其它的文件,这个遵循的原则是什么?谢谢

  • 您好!

    从你贴的error可以看出使用了intc的相关API。

    原则,你用了哪个模块的API就得添加相应的lib.

  • 打开一个工程,编译出现以下错误,是缺少哪个链接库  

     

    undefined            first referenced             symbol                  in file                                                                                                                               ---------            ----------------     _CACHE_clean         D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj  _CACHE_enableCaching

     D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj  _CACHE_setL2Mode    

     D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj  _CSLDM642_LIB_      

     D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj  _DAT_close           ..\lib\vport.l64<vportdis.o64>                                                                                                            _DAT_copy           

     D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj  _DAT_fill            ..\lib\vport.l64<vportdis.o64>                                                                                                            _DAT_open           

    D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj  _EDMA_allocTable     ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_clearChannel   ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_close          ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_config         ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_disableChannel ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_enableChannel  ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_freeTable      ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intAlloc       ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intClear       ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intDisable     ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intDispatcher  ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intEnable      ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intFree        ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_intHook        ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_link           ..\lib\vport.l64<vportcap.o64>                                                                                                            _EDMA_open           ..\lib\vport.l64<vportcap.o64>                                                                                                            _EMIFA_config        ..\lib\evmdm642bsl.lib<evmdm642.obj>                                                                                                      _GPIO_open           ..\lib\evmdm642bsl.lib<evmdm642.obj>                                                                                                      _I2C_bb              ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_config          ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_getConfig       ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_open            ..\lib\evmdm642bsl.lib<evmdm642.obj>                                                                                                      _I2C_outOfReset      ..\lib\evmdm642bsl.lib<evmdm642.obj>                                                                                                      _I2C_readByte        ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_rrdy            ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_sendStop        ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_start           ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_writeByte       ..\lib\vport.l64<_iic.o64>                                                                                                                _I2C_xrdy            ..\lib\vport.l64<_iic.o64>                                                                                                                _IRQ_clear           ..\lib\vport.l64<vportcap.o64>                                                                                                            _IRQ_disable         ..\lib\vport.l64<vportcap.o64>                                                                                                            _IRQ_enable          ..\lib\vport.l64<vportcap.o64>                                                                                                            _IRQ_globalDisable   ..\lib\vport.l64<vportcap.o64>                                                                                                            _IRQ_globalRestore   ..\lib\vport.l64<vportcap.o64>                                                                                                            _IRQ_map             ..\lib\vport.l64<vportcap.o64>                                                                                                            __CSL_init           D:\\software\\TS-AVoIP-64x Experiment\\TS-AVoIP-64x Experiments\\TS-AVoIP-64x_examples\\Lab6.2-DM642_image_DTC\\debug\\video_ntsc_pal.obj

    error: unresolved symbols remain error: errors encountered during linking; "./debug/DM642_image_DTC.out" not    built

    >> Compilation failure

    Build Complete,   1 Errors, 0 Warnings, 0 Remarks.

  • 你用的是DM642平台么,请把问题发到达芬奇子论坛,这里只管C64及keystone,谢谢。