你好
我有一块板子是参照hawkboard开发板(OMAP-L138)的原理图设计的,后来看了TI发表的声明说不推荐参照该设计,而且hawkboard开发板也给出了一个地方的修改,就是如下图所示。

它给出的声明是(The fix is made up by removing two ferrite beads and shortening the pads afterwards),就是去掉这两个磁珠并且短路。这两个磁珠是用来给DDR2的供电系统用的,如下图。
那么请问,这两个磁珠为什么要去掉?会产生哪些影响?
因为我目前板子出了点问题,就是如果保留磁珠的话,我能使用DDR2并且向NANDFLASH写入UBL,但是如果去掉磁珠的话,我就不能使用DDR2向NANDFLASH写入UBL了,但是可以使用OMAP-L138芯片内部的共享内存向NANDFLASH写入UBL。此时我应该怀疑是DDR2这里出了问题,但是我通过CCS4.2单独读写DDR2又没有任何问题,请问这是怎么回事呢?我如果再加上磁珠的话,马上就能写入UBL,但是后期烧写UBOOT和内核的时候会总是卡住,不稳定。所以强烈希望大家能帮帮我,这个问题已经困扰我很多天了,谢谢!