This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

667x的电路设计关于FT2232HL的配置问题



你好。我正在参照TMDXEVM6678L EVM开发板,进行6678的电路和PCB设计。因为客户要求,需要通过USB接口仿真6678,准备设计通过XDS100进行6678的USB-JTAG电路。在开发板的设计中,FT2232HL上电后通过AT93C46配置为JTAG模式,同时FT2232HL的B通道与6678的UART相连。我的问题是:

1 AT93C46如何进行配置,查询FT2232HL资料,eeprom里存储的是VID和PID,这个配置文件属于开发板的一部分,TI是否提供?

2 如问题1中,AT93C46能否通过usb在PC端进行配置,那么仅考虑FT2232HL与6678程序下载部分。

3 如有这方面的参考设计或参考文档,请给出名字和连接。十分感谢。

若无法提供,将开发板上的AT93C46内的的数据读出,烧写在新的EEPROM里装焊在设计的电路板中使用,是否可行?