如题
我是新下载安装的CCSV6.1,安装后自己新建了一个只有几行代码的小测试工程。芯片是C6748,编译器C6000,仿真器用的是XDS 100V2,XDS560PLUS两种。遇到了仿真器挂载后单步执行的按钮呈灰色。请问这是什么原因?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如题
我是新下载安装的CCSV6.1,安装后自己新建了一个只有几行代码的小测试工程。芯片是C6748,编译器C6000,仿真器用的是XDS 100V2,XDS560PLUS两种。遇到了仿真器挂载后单步执行的按钮呈灰色。请问这是什么原因?
从6.1.2的release notes里看,这个bug修复了,更新到CCS 6.1.2吧。
http://software-dl.ti.com/ccs/esd/CCSv6/latest/exports/ReleaseNote.htm
Bug Fixes
|
dbid |
Id |
Component |
Headline |
|
33606192 |
SDSCM00051760 |
C2000 Code Generation Tools |
Compiler error for missing brace "}" at end of source is not reported in Problems view |
|
33594903 |
SDSCM00040471 |
DVT |
Show profile data in call graph |
|
33606099 |
SDSCM00051667 |
DVT |
Graph export/import should save/restore autoscale and y-axis range settings. |
|
33606155 |
SDSCM00051723 |
DVT |
symbol names not show for EnergyTrace on MSP430 |
|
33606293 |
SDSCM00051861 |
DVT |
Improve EnergyTrace UI for power graph to clearly show whether measurements are relative or absolute |
|
33602008 |
SDSCM00047576 |
IDE |
Unable to generate code coverage data via DSS |
|
33602046 |
SDSCM00047614 |
IDE |
Scripting Console: Button to open/load a javascript file |
|
33602176 |
SDSCM00047744 |
IDE |
legacy format header files not handled correctly |
|
33602266 |
SDSCM00047834 |
IDE |
DS initiated progress dialog should consider the dialog option "Always Run on Background" |
|
33602278 |
SDSCM00047846 |
IDE |
Once I start a CCS debug session, build all will popup a modal progress box |
|
33602500 |
SDSCM00048068 |
IDE |
[C28 Flash] Flash programming does not work with "Auto Run on Reset" option on |
|
33602584 |
SDSCM00048152 |
IDE |
Importing a SYS/BIOS project created with older version of CCS causes migration errors |
|
33602609 |
SDSCM00048177 |
IDE |
Scan compiler options files to improve conditional formatting |
|
33602657 |
SDSCM00048225 |
IDE |
Flash programming sometimes results in error "Timed out while writing to Flash memory" |
|
33602680 |
SDSCM00048248 |
IDE |
Breakpoint on a single source line causes the debugger to break twice before resuming execution |
|
33602690 |
SDSCM00048258 |
IDE |
Importing a CCS3.3 library project with project dependencies results in java.lang.NullPointerException |
|
33602697 |
SDSCM00048265 |
IDE |
In the compiler selection drop-down the listing for gcc should include the executable name |
|
33602741 |
SDSCM00048309 |
IDE |
Missing .ebss and .reset directive highlights for C2000 cmd file |
|
33602776 |
SDSCM00048344 |
IDE |
Class members are not shown in Variables view for code built with GCC |
|
33602789 |
SDSCM00048357 |
IDE |
MSP430 Trace View does not refresh properly when decoding instructions |
|
33602816 |
SDSCM00048384 |
IDE |
Project import tool sometimes does not resolve paths correctly |
|
33602820 |
SDSCM00048388 |
IDE |
Provide more precise error messages in Import CCS Project wizard |
|
33602840 |
SDSCM00048408 |
IDE |
Switching between two projects can sometime get GUI Composer out of sync |
|
33602849 |
SDSCM00048417 |
IDE |
The compiler option -v that specifies the silicon version is retained when switching device variants |
|
33602878 |
SDSCM00048446 |
IDE |
Flashing fails on Stellaris TM4C129X devices |
|
33602894 |
SDSCM00048462 |
IDE |
Makefile validation errors prevent makefile re-generation |
|
33602900 |
SDSCM00048468 |
IDE |
The Location of local variables is sometimes displayed incorrectly for GCC ELF files |
|
33602985 |
SDSCM00048553 |
IDE |
Include paths using "workspace_loc: variable are not passed to the compiler if the path does not exist |
|
33603000 |
SDSCM00048568 |
IDE |
Request to have LCD option for meter widget |
|
33603001 |
SDSCM00048569 |
IDE |
Request to have an out of range indicator option for gauges and meters |
|
33603044 |
SDSCM00048612 |
IDE |
CCS fails to program certain .out files when "Auto ECC generation" is enabled in Flash Settings |
|
33603191 |
SDSCM00048759 |
IDE |
Deadlock due to "buddy" classloading |
|
33603338 |
SDSCM00048906 |
IDE |
Invoking gmake with -s option causes the Problems view to not update after errors have been corrected |
|
33603350 |
SDSCM00048918 |
IDE |
Would like a method to disable Optimization Advice |
|
33603434 |
SDSCM00049002 |
IDE |
App center in installer shows MSP430 content even when MSP not selected |
|
33603485 |
SDSCM00049053 |
IDE |
Request fpr Memory Allocation view to show UNION sections |
|
33605396 |
SDSCM00050964 |
IDE |
Hex Utility (and GNU Objcopy in the case of GNU tools) should run before post build steps in CCS |
|
33605484 |
SDSCM00051052 |
IDE |
When using SW breakpoints in source file, the LDR instruction does not work correctly on a Cortex-A8 (AM335x) |
|
33605678 |
SDSCM00051246 |
IDE |
User is prompted to terminate existing debug session when running a multi-session DSS script from the Console |
|
33605704 |
SDSCM00051272 |
IDE |
The CCS Online Help content for "Data File Formats" is outdated |
|
33605866 |
SDSCM00051434 |
IDE |
Multiple copies of the same header file are opened when clicking on a error/warning in the Problems view |
|
33605961 |
SDSCM00051529 |
IDE |
Debugserver should release files that are opened in the target application when a debug session is terminated |
|
33606052 |
SDSCM00051620 |
IDE |
TI-RTOS template project fails to build with GNU build tools |
|
33606056 |
SDSCM00051624 |
IDE |
DefaultToolChain property on Device XML files is not being properly acknowledged by the Project wizard |
|
33606059 |
SDSCM00051627 |
IDE |
Passing XDCROOT as a parameter to batch file in post build step does not work as expected |
|
33606063 |
SDSCM00051631 |
IDE |
CCS crash in a gcc compiled C++ program when expanding a class pointer |
|
33606075 |
SDSCM00051643 |
IDE |
Tiva E device support does not get installed |
|
33606136 |
SDSCM00051704 |
IDE |
90 day eval license activation is broken |
|
33606202 |
SDSCM00051770 |
IDE |
Closing and restarting CCS when in CCS Simple mode causes debugger to no longer work (all debug functions are grayed out) |