This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS6437如何配置访问单独的16bitDDR2?



项目需要,设计了一个DM6437的最小系统版,为了节约成本,板上只用了一片16位的DDR2芯片,查阅DM6437的数据手册,显示可以做16位使用,但是调了几天都没弄好,不知道要改那些寄存器?请问TI公司,有该款芯片16位DDR2访问的程序吗?

  • 配置SDBCR的NM位,不过这个都不知道的话,估计你时序也没有配置吧,当然不可能能通。

    还要根据DDR芯片手册的参数,按手册spru986里的说明对DDR时序进行计算配置。

  • 很感谢你的回复,我通过查阅DDR2芯片手册和spru986,对DDR2频率做了重新配置,由162Mhz降到135Mhz,目前程序能下载运行,但是不知道这个配置得到的135Mhz,我该如何验证,可不可以用示波器检测?或者说,通过寄存器查看结果?另外,对16bit访问,除了改   

     DDR_SDBCR = 0                   // DDR Bank Config
            | ( 0 << 23 )               // Boot unlock  = No
            | ( 2 << 19 )               // Reserved     = ( 2 )
            | ( 0 << 18 )               // Drive Strength= Normal
            | ( 3 << 16 )               // Reserved     = ( 3 )
            | ( 1 << 15 )               // Modify SDBCR = Yes
            | (1<< 14 )               // Bus width    = 16-bit
            | ( 4 << 9 )                // CAS latency  = 4
            | ( 3 << 4 )                // Bank Setup   = 8 banks
            | ( 2 << 0 );               // Page Size    = 1024-word / 10 column bits

    还需要改其他的吗?非常感谢

  • 能下载运行说明就差不多了,是否稳定就难说了,没见你有修改时序参数。


  • 感谢你的回复!

    我在配置的时候,先设置DDR2_CLK,通过以下代码设置为135Mhz


    Setup_PLL2_DDR_135_MHz_OscIn( )
    {
        /* [VPSS @54 MHz][DDR @135 MHz] w/ Onchip Oscillator */
        setup_pll_2( 0, 19, 9, 1 );
    }


    此后的时序代码控制如下:


    /* ------------------------------------------------------------------------ *
     *                                                                          *
     *  setup_ddr2( )                                                           *
     *      Configure DDR2 to run at specified frequency.                       *
     *                                                                          *
     *      Using 2 x MT47H64M16 - ( 8Mb x 16 bits x 8 banks ) @ 135 MHz        *
     *                                                                          *
     * ------------------------------------------------------------------------ */
    setup_ddr2( )
    {
        #define DDR_SDBCR           *( unsigned int* )( 0x20000008 )
        #define DDR_SDRCR           *( unsigned int* )( 0x2000000c )
        #define DDR_SDTIMR          *( unsigned int* )( 0x20000010 )
        #define DDR_SDTIMR2         *( unsigned int* )( 0x20000014 )
        #define DDR_DDRPHYCR        *( unsigned int* )( 0x200000e4 )

        #define DDR_VTPIOCR         *( unsigned int* )( 0x200000f0 )
        #define DDR_DDRVTPR         *( unsigned int* )( 0x01c42038 )
        #define DDR_DDRVTPER        *( unsigned int* )( 0x01c4004c )

        int dummy_read;
        int pch_nch;
        int freq = 135;
     int refresh_rate=0;

        GEL_TextOut( "Setup DDR2 (%d MHz + 32-bit bus)... ",,,,, freq );

        /*
         *  Step 1 - Setup PLL2
         *  Step 2 - Enable DDR2 PHY
         */
        psc_change_state( 13, 3 );

        /*
         *  Step 3 - DDR2 Initialization
         */
        DDR_SDBCR = 0                   // DDR Bank Config
            | ( 0 << 23 )               // Boot unlock  = No
            | ( 2 << 19 )               // Reserved     = ( 2 )
            | ( 0 << 18 )               // Drive Strength= Normal
            | ( 3 << 16 )               // Reserved     = ( 3 )
            | ( 1 << 15 )               // Modify SDBCR = Yes
            | ( 1 << 14 )               // Bus width    = 32-bit
            | ( 4 << 9 )                // CAS latency  = 4
            | ( 3 << 4 )                // Bank Setup   = 8 banks
            | ( 2 << 0 );               // Page Size    = 1024-word / 10 column bits


     DDR_DDRPHYCR = 0                // DDR PHY Control Register
            | ( 0x1400190 << 6 )        // Magic number
            | ( 0 << 5 )                // DLL release
            | ( 0 << 4 )                // DLL powered up
            | ( 4 << 0 );               // Read latency ( CAS + RT - 1 )
                                       

        DDR_SDTIMR = 0                  // DDR Timing Register
            | ( 17 << 25 )              // tRFC = ( 133.3 ns / 7.4 ns ) - 1
            | ( 2 << 22 )               // tRP  = (  22 ns / 7.4 ns ) - 1
            | ( 2 << 19 )               // tRCD = (  22 ns / 7.4 ns ) - 1
            | ( 1 << 16 )               // tWR  = (  15 ns / 7.4 ns ) - 1
            | ( 5 << 11 )               // tRAS = (  45 ns / 7.4 ns ) - 1
            | ( 8 << 6 )                // tRC  = (  67 ns / 7.4 ns ) - 1
            | ( 1 << 3 )                // tRRD = ( 10 ns / 7.4 ns ) - 1
            | ( 1 << 0 );               // tWTR = ( 10 ns / 7.4 ns ) - 1

        DDR_SDTIMR2 = 0                 // DDR Timing Register
            | ( 19 << 16 )              // tXSNR= ( 143.3 ns / 7.4 ns ) - 1
            | ( 199 << 8 )              // tXSRD= ( 200 - 1 ) cycles
            | ( 1 << 5 )                // tRTP = ( 7.5 ns / 7.4 ns ) - 1
            | ( 2 << 0 );               // tCKE = ( 3 - 1 ) cycles

        DDR_SDBCR    = 0x00130832;      // DDR Bank: cannot modify

        refresh_rate = ( freq * 78 ) / 10;

        DDR_SDRCR = 0
            | ( 0 << 31 )               // Exits self-refresh
            | ( 0 << 30 )               // Disable MCLK stopping
            | refresh_rate;             // Refresh Control = 7.8 usec * freq

        /*
         *  Step 4 - Dummy Read from DDR2
         */
        dummy_read = *( int* )0x80000000;

        /*
         *  Step 5 - Soft Reset ( SYNCRESET followed by ENABLE ) of DDR2 PHY
         */
        psc_change_state( 13, 1 );
        psc_change_state( 13, 3 );

        /*
         *  Step 6 - Enable VTP calibration
         *  Step 7 - Wait for VTP calibration ( 33 VTP cycles )
         */
        DDR_VTPIOCR = 0x201f;
        DDR_VTPIOCR = 0xa01f;
        _wait( 1500 );

        /*
         *  Step 8 - Enable access to DDR VTP reg
         *  Step 9 - Reat P & N channels
         *  Step 10 - Set VTP fields PCH & NCH
         */
        DDR_DDRVTPER = 1;
        pch_nch = DDR_DDRVTPR & 0x3ff;
        DDR_VTPIOCR = 0xa000 | pch_nch;

        /*
         *  Step 11 - Disable VTP calibaration
         *          - Disable access to DDR VTP register
         */
        DDR_VTPIOCR &= ~0x2000;
        DDR_DDRVTPER = 0;

        GEL_TextOut( "[Done]\n" );
    }


    如此,得到16bit,DDR2_CLK=135Mhz的配置,不知道是否合适?

    下载调试的时候,采用的是LED闪烁程序,程序的cmd文件,将代码放在DDR2运行。实验结果正常,没出现问题,这是否说明配置成功?

  • dan li1 说:

    DDR_DDRPHYCR = 0                // DDR PHY Control Register
            | ( 0x1400190 << 6 )        // Magic number
            | ( 0 << 5 )                // DLL release
            | ( 0 << 4 )                // DLL powered up
            | ( 4 << 0 );               // Read latency ( CAS + RT - 1 )
                                       

        DDR_SDTIMR = 0                  // DDR Timing Register
            | ( 17 << 25 )              // tRFC = ( 133.3 ns / 7.4 ns ) - 1
            | ( 2 << 22 )               // tRP  = (  22 ns / 7.4 ns ) - 1
            | ( 2 << 19 )               // tRCD = (  22 ns / 7.4 ns ) - 1
            | ( 1 << 16 )               // tWR  = (  15 ns / 7.4 ns ) - 1
            | ( 5 << 11 )               // tRAS = (  45 ns / 7.4 ns ) - 1
            | ( 8 << 6 )                // tRC  = (  67 ns / 7.4 ns ) - 1
            | ( 1 << 3 )                // tRRD = ( 10 ns / 7.4 ns ) - 1
            | ( 1 << 0 );               // tWTR = ( 10 ns / 7.4 ns ) - 1

        DDR_SDTIMR2 = 0                 // DDR Timing Register
            | ( 19 << 16 )              // tXSNR= ( 143.3 ns / 7.4 ns ) - 1
            | ( 199 << 8 )              // tXSRD= ( 200 - 1 ) cycles
            | ( 1 << 5 )                // tRTP = ( 7.5 ns / 7.4 ns ) - 1
            | ( 2 << 0 );               // tCKE = ( 3 - 1 ) cycles

     

    这几个参数要对照你采用的DDR芯片的手册里的数据比较一下,确保稳定。