DM6446的USB接口包括一个VBUS信号,如果我将USB接口作为一个HOST接口使用时,VBUS接口一定要连接5V电源吗?还是只要给出一个5V的信号就可以?
USB和WIFI模块相接,WIFI模块的电压是3.3V。这种情况下VBUS是否可以悬空处理?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM6446的USB接口包括一个VBUS信号,如果我将USB接口作为一个HOST接口使用时,VBUS接口一定要连接5V电源吗?还是只要给出一个5V的信号就可以?
USB和WIFI模块相接,WIFI模块的电压是3.3V。这种情况下VBUS是否可以悬空处理?
你好,
你可以在DM6446的数据手册里面找到下面的信息:
USB_VBUS
5-V input that signifies that VBUS is connected.
When the USB peripheral is not used, the USB_VBUS signal should be either pulled down or pulled up via a 10-kW resistor.