HI,TI工程师们,我这边有一些关于DVRRDK缩放器问题需要请教。
环境:DM8168CCYG4
DVRRDK 04.00.00.03
1.缩放器限制
如上连接中提到,Note that only 4 scalers can be used simultaneously if scalers are used in m2m mode.You can use 5 scalers if you use one of the scalers in displayWB mode. ie.HDMI output is written back to memory.如果使用m2m模式,有4个缩放器可以同时使用。如果让其中一个工作在显示回写的模式下,可以使用5个缩放器。
如上连接中提到:
Yon can not have
SYSTEM_SW_MS_SC_INST_VIP0_SC & SC5 at the same time
also
Not possible to have
SYSTEM_SW_MS_SC_INST_VIP1_SC & SEC path SD display simultaneously