This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Keystone 1开发软件包LTE应用的问题



(1)请问K1_SKT_v1.1中AIF2_LTE_FDD和TDD的例程是不是不包含调制和信道编码的代码?我是初学者,找了半天没找到OFDM调制或者CRC、Turbo编码相关的代码。我开始以为AIF2的例程需要和FFTC的例程联用才能实现OFDM信号的产生,但是K1_SKT_v1.1的开发软件包中未包含FFTC的例程。

(2)关于TCP3D例程的使用,请问如果用6614的板子TMDXEVM6614LXE,需要将keystone_TCP3D.c中的gtTcp3dInstInfo的值如何修改才能使用?

下面是keystone_TCP3D.c中对gtTcp3dInstInfo的赋值

const T_TCP3D_InstInfo gtTcp3dInstInfo[NUM_TCP3D] = {
{
(Uint32)CSL_PSC_PD_TCP3D_A,
(Uint32)CSL_PSC_LPSC_TCP3D_A,
(CSL_Tcp3d_cfgRegs *)CSL_TCP3D_A_CFG_REGS,
(Uint32)CSL_TCP3D_A_DATA_REGS,

(Uint8)2,
{
(Uint8)CSL_TPCC2_TCP3D_A_REVT0,
(Uint8)CSL_TPCC2_TCP3D_A_REVT1,
}
}, /* TCP3D_0 */
{
(Uint32)CSL_PSC_PD_TCP3D_B,
(Uint32)CSL_PSC_LPSC_TCP3D_B,
(CSL_Tcp3d_cfgRegs *)CSL_TCP3D_B_CFG_REGS,
(Uint32)CSL_TCP3D_B_DATA_REGS,

(Uint8)2,
{
(Uint8)CSL_TPCC2_TCP3D_B_REVT0,
(Uint8)CSL_TPCC2_TCP3D_B_REVT1,
}
}, /* TCP3D_1 */