This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678的PCIE与PC机之间通信



  各位TI高手,请教下如下问题:

   现在我使用我公司研发的一块C6678板卡,上面带了一块8648的PCIE桥芯片,因此c6678的PCIE是通过了桥芯片与PC机通信,C6678做从,使用TI提供的PCIEExample工程进行测试,我先对板卡上电,程序先跑起来,然后开PC机,接着程序里也显示LINKUP上了,PC机进入WINDOWS后,也能在设备管理器里找到C6678这块板卡设备,但是没有分配中断和资源,不能通过BAR1空间异步读写C6678的内存或DDR3。使用WinDrver来看,里面相关寄存器也配置了的,请问下有没有高手知道这是怎么回事,未什么PC机没有给分配资源了,是没有分配资源造成不能异步访问吗?

    急啊,希望有TI相关人士来解答下!