This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8127内核供电&工作频率关系



DM8127内核供电&工作频率关系如表格所示,但是表格中提到在给定CORE电压之后ARM,DSP,HDVICP电压之间供电是否要按照表格8-5进行供电;

我现有板子CORE=1.2V(DDR400),ARM=1.09V(ARM-600M),DSP=1.35V(DSP-750M),HDVICP=1.35V(HDVICP-450M),这样供电是否可以?

现板子已工作4天都没发现有什么问题,但是不知道是否有其他隐藏的问题;是否可以按照现有供电方式进行设计,默认生产?

  • 你好,

    1. 你使用的频率必须在你使用的芯片支持的最高频率范围内。

    2. 只有在table8-5里面的组合TI是在芯片上测试过,能保证长时间稳定运行。其他组合,TI无法保证能保证长时间稳定运行。