手头有一个AM3359的ICE,开始使用UART5作为输出端口,用USB连接到电脑可以在超级终端或者Term输出信息(裸机程序实现的)。
但是现在突然不能输出了,用线把UART5引脚引出来(下图蓝色方框的地儿)用示波器测试,发现没有输出信息,猜测可能是UART芯片坏了,有能帮忙确认一下吗,是否是UART芯片坏了,还是别的原因?
如果确实是UART芯片坏了,我想输出,是否可是使用CAN,I2C等串口端口吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
后来用UART4端口引出一个UART,用MAX3221转换成232,输出是乱码,后来调查是忘记加了下拉电阻,加上之后输出正常。
请问用UART4串口,UARTecho 范例中的代码要怎么改写呢?