This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

stk_6657下的工程编译问题 急急急!!!



你好 我自建工程 编译STK_C6657下的UART时 提示如下: #20 identifier "CSL_INTC0_UARTINT1" is undefined UART_Interrupt.c #20 identifier "CSL_INTC0_URXEVT1" is undefined UART_Interrupt.c 显然是\pdk_C6657_1_1_1_4\packages\ti\csl中的头文件没有定义变量 是不是我的PDK版本不对啊 我用的是“pdk_C6657_1_1_1_4”,应该使用哪一个版本的PDK???在哪里有了??? 谢谢了!