1、请问PLL中的输入时钟是由谁提供的?在TMDXEVM6678L上具体是固定值吗,是多少?下表中的Input Clock Freq又是指的什么?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、请问PLL中的输入时钟是由谁提供的?在TMDXEVM6678L上具体是固定值吗,是多少?下表中的Input Clock Freq又是指的什么?

楼主所贴的表我现在也很疑惑,版主的回答也太随意了,一句请参考技术手册就完事了。。。表中列出的多个时钟源好像都是给内核时钟源的,从表中的参数计算正好符合列出的时钟频率。但我自己测试了PLL的设置(PLLM和PLLD),并用示波器测量了TP12管脚,发现内核时钟源是固定的100MHz,又看了硬件设计图,并没有表中体现的多个时钟源。还请版主解惑下。。
既然已经固定时钟源了,那表的第一项BOOTMODE[12:10]有什么用呢,管脚不按那个值配置,得出来的时钟也还是100MHz。
另:二次配置PLLD PLLM应该可以,调试时GEL配置过PLLM,PLLD,有的示例程序中又重新配置过
1 对啊,我也在疑惑这个问题,求版主解答。。。。urgent.
"既然已经固定时钟源了,那表的第一项BOOTMODE[12:10]有什么用呢"!
2 是不是应该根据自己板子上的时钟来设置BOOTMODE[12:10],比如时钟如果是80M就用0b010,EVM6678板是100M的就应该用0b011。
那我的时钟如果不在这所列的8个时钟内,就得自己找个相近的值设置这三个管脚。
33如果上面说的正确,可以猜测,DSP的ROM code(bootloader)是根据BOOTMODE[12:10]这三个引脚的值来配置PLLD PLLM的
望大家帮忙