打开capture的tiler
capturePrm->tilerEnable = TRUE;/
然后系统报错
[m3vpss ] 24407: Assertion @ Line: 1605 in utils/src/tile_alg_binpack.c: tilerAddr != UTILS_TILER_INVALID_ADDR : failed !!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
打开capture的tiler
capturePrm->tilerEnable = TRUE;/
然后系统报错
[m3vpss ] 24407: Assertion @ Line: 1605 in utils/src/tile_alg_binpack.c: tilerAddr != UTILS_TILER_INVALID_ADDR : failed !!!
如果capturelink 输出设置为yuv422I,tiler 设置为disable呢?
如果capture设置为422i tiler disable的话 是没有问题的 不会有屏幕顶部的条纹闪烁
但是由于我们要简化业务图,所以直接用capture出420进行编码,这样的话,屏幕顶部闪烁,但是我们发现tiler = true 就不会闪
因此想使用tiler = ture
在rdk demo上这样设置是可以的,但是自己的业务图会发生这样的错误
[m3vpss ] 24407: Assertion @ Line: 1605 in utils/src/tile_alg_binpack.c: tilerAddr != UTILS_TILER_INVALID_ADDR : failed !!!