OMAP4460里的DSP可以编程吗? 有没有相关的资料或教程? 谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那该怎么使用4460里的DSP呢? 请问在哪里可以找到相关的资料? 谢谢
可不可以像 OMAP-L138的DSP开发那样实现ARM和DSP之间的通信呢? 谢谢?
Ubuntu 12.04 可以吗?
OMAP4460里的DSP一般情况下是怎么使用的? 谢谢
Let me check and get back to you
我看到这样的说法
We have not opened Tesla DSP source code to customers to program their own applications and we have no plan to support customers who independently try to use the DSP in standalone mode.
所以应该不能用了
谢谢你。
那4460里的DSP是芯片内部自己使用使用时的了?
是不是说如果我装了Linux 系统,并且可以驱动DSP起来,在数据运算时,如果需要用到DSP,系统会自己调用DSP?
Please take a look on following sources:
elinux.org/.../DSP_Howto
omappedia.org/.../DSPBridge_Project
gforge.ti.com/.../frs