This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

在线等:C66x Relocation Overflow



我们在C6678上编译一个大型的C++程序,环境是CCS 6.1,使用JTAG把程序“裸跑”在一个C66x core上。但因为程序代码量比较大,出现下列warning:

#17003-D</a>  relocation from function "getGlobalMatOpInitializer" to symbol "$P$T427$1" overflowed; the 16-bit relocated address 0xdcf4 is too large to encode in the 15-bit unsigned field (type = 'R_C6000_SBR_U15_B' (11), file = "./src/core/matop.obj", offset = 0x00005e04, section = ".text") cvdef.h /cppTest/src/core line 214 C/C++ Problem

请问要怎样才能支持一个大型的C++程序呢?

Remedy

  1. Use trampolines (if available)
  2. Use a large code (or data) memory model
  3. Make the code size smaller
  4. Modify the linker command file to place the calling function closer to the called function.

已经尝试过如下工程选项:--trampolines=on --mem_model:const=far --mem_model:data=far,另外不希望采用第3、4种方式。

谢谢!