This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

配置sitara sdk的问题



sdk版本是ti-processor-sdk-linux-am335x-evm-01.00.00.00,板子用的BB Black 用板子上的ttl串口转成rs232连到host,安装完SDK后运行setup.sh时遇到提示:

...

No BeagleBone (Black) or StarterKit detected. Assuming
general purpose evm is being used. Is this correct?
(y/n) n

Please connect the Beaglebone (Black) or StarterKit to the PC
If your using the StarterKit board make sure it is turned on
Press any key to try checking again.

No BeagleBone (Black) or StarterKit detected. Assuming
general purpose evm is being used. Is this correct?
(y/n) n

看了一下setup.sh,里面会用<SDK version>/bin/setup-uboot-env.sh 检查目标板的连接情况,相关的代码如下:

....

# Now let's check for BeagleBone Black
    sudo lsusb -vv -d 0403:6001 > /dev/null
   
    if [ "$?" = "0" ]
    then
        isBB="y"
        isBBBlack="y"
        return
     fi

.....

0403:6001应该是FTDI的usb转串口设备,我没用这个设备连接BBB板子,所以会提示找不到BBB目标板,

我的问题是,要是我修改setup-uboot-env.sh文件里判断转串口设备号的条件,比如我有个PL2303的usb转串口设备,VID/PID是067b:2303,我改成检测这个设备是否就能正常工作而且没有什么其它隐患?我尝试修改后确实能继续往下配置,就是不知道这样做会有什么不良后果,毕竟它只是检测了一个转接设备,我甚至没连接目标板,只是插上了usb转串口设备,就能提示我连接了一个BBB或者EVM-sk。