This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6638 QM1与QM2的Queue之间如何传递Host Packet Descriptor



Ti专家:

       你们好!

       目前我在使用6638芯片,想利用Queue设计8个Core之间通信的机制,QM1的Queue和QM2的Queue之间需要互传Host Packet descriptor,测试发现属于同一QM的Queue之间可以正常互传Host Packet Descriptor,但不同的QM间的Queue就不能完成Host Packet Descriptor的互传。

       配置如下:

       1)发送Queue使用QM2的8992;

       2)QM2 FlowID=1 的配置为: RXFlow N Configuration RegisterA寄存器:RX_DEST_QMGR=0和RX_DEST_QNUM=652(QM1的pendQ);

       3)Host packet Descriptor中SourceTag- Lo=1(QM2的FlowID号);

        将Host packet descriptor push到queue8892,发现QM1的652不能收到descriptor,QM2的652(Queue8844)收到了descriptor。

        我仔细看了sprugr9h.pdf/1.9节,好像在说这种使用情况,没看明白,请你们帮忙解释一下;另外如何解决QM1和QM2 Queue互传descriptor,希望能得到你们的建议。

  

  • 确认Global control register region中的QM0~3 base address register已按手册配置。

  • 感谢Andy的回复,我核对了一下代码,已经按手册的推荐设置进行了配置,下面是截取的部分代码,不同QM之间仍然不能实现相互通信,不知道配置是否存在问题或者遗漏。

    #define QM1_BASE_ADDRESS (0x34020000)
    #define QM2_BASE_ADDRESS (0x34030000)
    #define QM3_BASE_ADDRESS (0xFFFFFFFF)
    #define QM4_BASE_ADDRESS (0xFFFFFFFF)
    #define MAX_QM_NUM 2
    #define QMSS_CFG_PKTDMA_BASE_OFFSET  (0x02000)


            for(i=0; i<MAX_QM_NUM; i++)
            {
                pstGblCfgRegs = (CSL_Cppidma_global_configRegs *)((uint8 *)pstGblCfgRegs + i * QMSS_CFG_PKTDMA_BASE_OFFSET);
                CSL_FINS(pstGblCfgRegs->EMULATION_CONTROL_REG,
                          CPPIDMA_GLOBAL_CONFIG_EMULATION_CONTROL_REG_LOOPBACK_EN, (uint32)1);
               
                /* Priority Control Register: RX_PRIORITY, TX_PRIORITY */
                CSL_FINS(pstGblCfgRegs->PRIORITY_CONTROL_REG,
                          CPPIDMA_GLOBAL_CONFIG_PRIORITY_CONTROL_REG_TX_PRIORITY, g_stQmDmaGlobalConfig[enPktDmaType].uiTxPriority);

                CSL_FINS(pstGblCfgRegs->PRIORITY_CONTROL_REG,
                          CPPIDMA_GLOBAL_CONFIG_PRIORITY_CONTROL_REG_RX_PRIORITY, g_stQmDmaGlobalConfig[enPktDmaType].uiRxPriority);

                pstGblCfgRegs->QM_BASE_ADDRESS_REG[0] = QM1_BASE_ADDRESS + i * 0x20000;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[1] = QM2_BASE_ADDRESS + i * 0x20000;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[2] = QM3_BASE_ADDRESS;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[3] = QM4_BASE_ADDRESS;
            }

  • 你配的是K1的,对K2,需要配置0x23a80000,0x23a90000,0x23aa0000, 0x23ab0000, 请对照k2 navigator user guide说明重配。

  • Andy,已经按照你的建议对代码做了修改,但测试发现QM0中的descriptor不能通过QM0的TxQueue\FlowID发送给QM1;

    修改后的代码如下:

    #define QM1_BASE_ADDRESS (0x23a80000)
    #define QM2_BASE_ADDRESS (0x23a90000)
    #define QM3_BASE_ADDRESS (0x23aa0000)
    #define QM4_BASE_ADDRESS (0x23ab0000)
    #define MAX_QM_NUM 2
    #define QMSS_CFG_PKTDMA_BASE_OFFSET  (0x02000)

     

            for(i=0; i<MAX_QM_NUM; i++)
            {
                pstGblCfgRegs = (CSL_Cppidma_global_configRegs *)((uint8 *)pstGblCfgRegs + i * QMSS_CFG_PKTDMA_BASE_OFFSET);
                CSL_FINS(pstGblCfgRegs->EMULATION_CONTROL_REG,
                          CPPIDMA_GLOBAL_CONFIG_EMULATION_CONTROL_REG_LOOPBACK_EN, (uint32)1);
               
                /* Priority Control Register: RX_PRIORITY, TX_PRIORITY */
                CSL_FINS(pstGblCfgRegs->PRIORITY_CONTROL_REG,
                          CPPIDMA_GLOBAL_CONFIG_PRIORITY_CONTROL_REG_TX_PRIORITY, g_stQmDmaGlobalConfig[enPktDmaType].uiTxPriority);

                CSL_FINS(pstGblCfgRegs->PRIORITY_CONTROL_REG,
                          CPPIDMA_GLOBAL_CONFIG_PRIORITY_CONTROL_REG_RX_PRIORITY, g_stQmDmaGlobalConfig[enPktDmaType].uiRxPriority);

                /* QMn Base Address Register:queue(0~4094) are set to QM0, queue(4096~8190) are set to QM1 */
                #if 0
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[0] = QM1_BASE_ADDRESS + i * 0x20000; //0x23a80000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[1] = QM2_BASE_ADDRESS + i * 0x20000; //0x23a90000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[2] = QM3_BASE_ADDRESS;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[3] = QM4_BASE_ADDRESS;
                #else
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[0] = QM1_BASE_ADDRESS; //0x23a80000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[1] = QM2_BASE_ADDRESS; //0x23a90000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[2] = QM3_BASE_ADDRESS;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[3] = QM4_BASE_ADDRESS;
                #endif
            }

     

            //fill the info of flowCfg.
            s_stInterCoreRxFlowCfg[i].usSopOffset = 0;
            s_stInterCoreRxFlowCfg[i].usDestQnum = 652;(s_stInterCoreRxAttr.stQueResource.stRxQueObj.usQueId)&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucDestQmgr = 1;//(s_stInterCoreRxAttr.stQueResource.stRxQueObj.usQueId>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].bPsLocation = FALSE;//tail
            s_stInterCoreRxFlowCfg[i].ucDescType = QUEMGR_HOST_PACKET;
            s_stInterCoreRxFlowCfg[i].bErrorHandling = TRUE;//Starvation errors result in subsequent re-try of the descriptor allocation operation.
            s_stInterCoreRxFlowCfg[i].bPsinfoPresent = FALSE;
            s_stInterCoreRxFlowCfg[i].bEinfoPresent = FALSE;
            s_stInterCoreRxFlowCfg[i].ucDestTagLo = 0;
            s_stInterCoreRxFlowCfg[i].ucDestTagHi = 0;
            s_stInterCoreRxFlowCfg[i].ucSrcTagLo = 0;
            s_stInterCoreRxFlowCfg[i].ucSrcTagHi = 0;
            s_stInterCoreRxFlowCfg[i].ucSizeThreshEn = 0x0f;//use threshold.
            s_stInterCoreRxFlowCfg[i].ucDestTagLoSel = QUEMGR_PKTDMA_RXFLOW_DSTTAG_OVERWRITE_WITH_DESC_DST_TAG_LO;
            s_stInterCoreRxFlowCfg[i].ucDestTagHiSel = QUEMGR_PKTDMA_RXFLOW_DSTTAG_OVERWRITE_WITH_DESC_DST_TAG_HI;
            s_stInterCoreRxFlowCfg[i].ucSrcTagLoSel = QUEMGR_PKTDMA_RXFLOW_SRCTAG_OVERWRITE_WITH_FLOWID;
            s_stInterCoreRxFlowCfg[i].ucSrcTagHiSel = QUEMGR_PKTDMA_RXFLOW_SRCTAG_OVERWRITE_WITH_DESC_SRC_TAG;
            s_stInterCoreRxFlowCfg[i].usSizeThresh0 = INTERCORERX_MSGSIZE_THRESH;
            s_stInterCoreRxFlowCfg[i].usSizeThresh1 = INTERCORERX_MSGSIZE_THRESH;
            s_stInterCoreRxFlowCfg[i].usSizeThresh2 = INTERCORERX_MSGSIZE_THRESH;
            s_stInterCoreRxFlowCfg[i].ucFdq1Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq1Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucFdq2Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq2Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucFdq3Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq3Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucFdq0Sz0Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq0Sz0Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucFdq0Sz1Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq0Sz1Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucFdq0Sz2Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq0Sz2Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);
            s_stInterCoreRxFlowCfg[i].ucFdq0Sz3Qmgr = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i]>>12)&(0x03);
            s_stInterCoreRxFlowCfg[i].usFdq0Sz3Qnum = (s_stInterCoreRxAttr.stQueResource.usTxFdqId[i])&(0xFFF);

            s_stInterCoreRxAttr.stQueResource.stQmssRxFlowObj[i].pstFlowCfg = &s_stInterCoreRxFlowCfg[i];

            if (QueMgrDrv_qmssRxFlowIdOpen(&s_stInterCoreRxAttr.stQueResource.stQmssRxFlowObj[i]))//s_stInterCoreRxAttr.stQueResource.stQmssRxFlowObj
            {
                g_stInterCoreOms.uiAllocRxFlowIdFailed++;
                //To do:close the opened queue and flowId.
                return;
            }

     

    其中

                #if 0
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[0] = QM1_BASE_ADDRESS + i * 0x20000; //0x23a80000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[1] = QM2_BASE_ADDRESS + i * 0x20000; //0x23a90000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[2] = QM3_BASE_ADDRESS;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[3] = QM4_BASE_ADDRESS;
                #else
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[0] = QM1_BASE_ADDRESS; //0x23a80000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[1] = QM2_BASE_ADDRESS; //0x23a90000 Keystone II
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[2] = QM3_BASE_ADDRESS;
                pstGblCfgRegs->QM_BASE_ADDRESS_REG[3] = QM4_BASE_ADDRESS;
                #endif

    两种方式都做了测试,我进行代码跟踪,发往结果发现:

    QM0和QM1 652 QUEUE_STATUS_CONFIG_REG_A 都显示为0,没收到信息。

    若将flow设置更改为 s_stInterCoreRxFlowCfg[i].ucDestQmgr = 0;//(s_stInterCoreRxAttr.stQueResource.stRxQueObj.usQueId>>12)&(0x03);

    QM0的 652可以收到信息;