TMS320C6678的NMI可以人为的触发吗?是几号引脚,可以通过CCSV5用软件来触发吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Smitch Jasom
可以通过硬件管脚或者内部寄存器来触发.
通过NMI pin,管脚M25,6678手册第180页有描述寄存器。
通过NMI Even Generation to CorePac (NMIGRx) Register寄存器来软件触发。
Thanks,
Liang
您好:
我在6678模拟环境下调用CSL_IPC_genNMIEvent函数对NMICGx寄存器写1,触发NMI中断,但是没有成功,目标核没能响应中断,不知道是什么原因。有没有可能是CSL_INTC_VECTID_NMI对应的event号不对,用ipc_local对应的91#或者1#都无法产生中断,不知道什么原因,您能指导一下吗,谢谢!
simulator有些功能没有实现,由于中断行为和硬件相关性较强,是产生中断相关的操作可能只实现了一小部分,您可以在开发板上测试一下看看结果。