This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

仿真的时候出错怎么办 啊?



Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during
the connect returned bad status or an error.
The cause may one or more of: invalid emulator serial number,
blank emulator EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the emulator can be located.
(Emulation package 5.1.450.0)

  • 仿真器链接不上板子,首先要考虑到CCS软件问题,即CCS仿真驱动是否有问题。其次是targetconfiguration配置,最后是板子以及仿真器硬件问题。可以做点交叉实验。另外c2000的问题,建议到C2000版块问问。