This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8168 usb转网口性能问题



我的软件版本的是rdk4.03的,linux的版本是2.6.37的,用了两块8168的板子通过usb相连,两块板子都是使用的是usb转网口驱动,当作网口来处理,一块板子采集视频通过usb网口传给另外一块板子,但是发现传输过程中丢包严重,比以太网口还严重,然后用ping -s pack_size在usb网口做测试,发现只要pack_size大于2k就ping不通,在ping该端口再也ping不通,两边都是这样的

然后我看了开机log有下面的信息

g_ether gadget: reset eem
usb0: gether_disconnect
g_ether gadget: init eem
g_ether gadget: activate eem
musb-hdrc periph: enabled ep1in for bulk IN, dma, maxpacket 512
musb-hdrc periph: enabled ep1out for bulk OUT, dma, maxpacket 512
usb0: qlen 10

如果我先改maxpacket这个值在哪里改呢,如果与这个没关系又是怎么回事呢?????????????????????????????????????????????????????????????????????????????????????

  • 在测试丢包过程中,A8的loading是否偏高呢?

    DM81xx PSP 的性能报告可以参考:http://processors.wiki.ti.com/index.php/TI81XX_PSP_04.04.00.02_Feature_Performance_Guide?keyMatch=PSP%2004.04&tisearch=Search-EN

  • A8的loading是正常的,怀疑可能硬件有问题

  • 还有一个问题就是usb转换成网口后,ping 1k的包就能ping通,但是ping 2k的包就不能ping通,这个是怎么回事呢??????????????????????????????????????????????????????????????????????????????????????????