This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6748 设置DSP/bios后报错,请帮忙解决下。谢谢




**** Build of configuration Debug for project test ****

"E:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
'Building target: test.out'
'Invoking: C6000 Linker'
"E:/ti/ccsv5/tools/compiler/c6000_7.4.4/bin/cl6x" -mv6740 --abi=coffabi -g --define=c6748 --display_error_number --diag_warning=225 --diag_wrap=off -z --stack_size=0x800 -m"test.map" --heap_size=0x800 -i"E:/ti/ccsv5/tools/compiler/c6000_7.4.4/lib" -i"E:/ti/ccsv5/tools/compiler/c6000_7.4.4/include" -i"E:/ti/bios_5_42_01_09/packages/ti/rtdx/lib/c6000" -i"E:/ti/bios_5_42_01_09/packages/ti/bios/lib" --reread_libs --warn_sections --display_error_number --diag_wrap=off --xml_link_info="test_linkInfo.xml" --rom_model -o "test.out" -l"./testcfg.cmd"  "./testcfg_c.obj" "./testcfg.obj" "./main.obj" -l"libc.a" -l"G:\CCS_WORK5.5\GNSS_WORK\DSP_PRJ\lib\Platform.lib" -l"G:\CCS_WORK5.5\GNSS_WORK\DSP_PRJ\lib\DSPLib\dsplib.ae674" -l"G:\CCS_WORK5.5\GNSS_WORK\DSP_PRJ\lib\system_config.lib" -l"G:\CCS_WORK5.5\GNSS_WORK\DSP_PRJ\lib\drivers.lib"
<Linking>

 undefined         first referenced
  symbol               in file     
 ---------         ----------------
 _GPIODirModeSet   ./main.obj      
 _GPIOPinWrite     ./main.obj      
 _PSCModuleControl ./main.obj      

error #10234-D: unresolved symbols remain

>> Compilation failure
error #10010: errors encountered during linking; "test.out" not built
gmake: *** [test.out] Error 1
gmake: Target `all' not remade because of errors.

**** Build Finished ****