This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用BIOS后VCP2多次转换后卡住的问题



之前在调VCP2,使用的是社区里找到的例程,现在移植到我们的工程里后出现了问题

作为一个单独的工程时,没有使用BIOS,循环执行vcp2译码是正常的,但是在我们的工程里是使用BIOS的,执行一定次数的vcp译码之后程序会跑到一个:

pdk_build_6670_1_1_2_6/gtcsl_platform/TurboNyquist/ti/csl/src/intc/_csl_intcIsrDispatch.asm

这个文件里,同时从异常状态寄存器里可以看到EFR的IXF位置1,IERR的值为1,从找到的资料中查到的异常说明是取指令错误。

在_csl_intcIsrDispatch.asm里是停在如下位置:
__CSL_intcIsrNMI:   
    CALLDISP 1
在这里单步执行后,跳转到一个_csl_intcIsrDispatch.asm文件中的这个位置:
__CSL_intcNmiDummy:
    b nrp
    nop 5   
接着就又跳回到第一个asm文件里了,一直就是这样在循环。

从开始不断循环译码到出现异常的执行次数不定,有时候几次就出现异常,最多可以循环执行两千多次。

不知道能否指点一下查找错误的思路

谢谢!