This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6000使用TSC测时间问题



您好:

       最近在测试C6678各模块运行时间中发现如下问题:

       测量DMA在DDR3中转置搬数时间的时候,使用gel文件初始化和使用keystone程序初始化pll这两种情况下,测出的时间不一致。

       查看两种环境下的主时钟和DDR3时钟,配置参数是一致的,且测量SRIO模块在DDR3中的传输时间和在DDR3中for循环写数的时间在两种环境化下是一致的,目前只有DMA转置传输时时间不一致,查看gel文件中关于DMA的设置并没有什么特别之处。

        求大神给点思路,以便排查问题

                                                                                                                                                                             thank  you

  • 测量差距有多大,DDR的初始化也是完全一样么?

  • 你好Andy:

          确实是DDR配置问题,我们这个片子只挂载了两片DDR,我把位宽设置成16bit了,所以速率只有gel环境下的差不多一半。

          有些地方我还是不太明白,为什么位宽少一半,两片DDR和四片DDR只在容量上有差异,在速率上差异很小(我在4DDR的板子上测量的时间和2DDR上基本一致)。

          而且在其他访问DDR的操作都没有发现两个初始化环境速率上的差异,只在DMA转置时出现。

         另外还有如下疑惑:

         1.如何测量DDR速率才是合理的???

         2.如果SRIO,HYPERLINK,DMA和CPU会同时访问DDR,这种情况会不会对DDR的访问效率有较大影响,如何优化配置???

     

                                                                                                                                                                                                           非常感谢!!!