This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678的一些问题



买的EVM板子,自制板子要准备备料了   

  1,如何区分PG1和PG2

  2,关于两种电源方案,数控和模拟优劣,哪种更好些

  3,EMIF16接Nor的启动方式,应该接在CS2吗?为什么论坛上有说CS2,但地址却说出的是0x70000000,0x70000000的地址不是CS0吗?

  4,Boot Parameter Table没搞清楚,为什么EVM板子带的eeprom51.bin的开始有很多个表而且是一样的

在这个地址开始不重复前面的table,这一块是什么内容,格式是怎么样的

下面这个是Boot Dev Addr,The I2C device address to boot from对应的地址,格式是什么样的

 为什么后面yes Configured Through Boot
Configuration Pins,这个和Pin有什么关系,这不是Boot Parameter Table吗