请问:现在我需要使用ADS131e04芯片将模数转换口的数字信号通过spi口送给C6748(spi0)进行处理。
1、我看ADS131e04芯片的手册上,该芯片是24bit的?采样速率为1、2、4、8、12、32、64KSPS,可调还是说自适应的?
2、在硬件设计时,ADS131e04芯片采样速率如何设置?
3、为了使ADS131e04芯片采样速率和C6748匹配,C6748的时钟如何考虑?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问:现在我需要使用ADS131e04芯片将模数转换口的数字信号通过spi口送给C6748(spi0)进行处理。
1、我看ADS131e04芯片的手册上,该芯片是24bit的?采样速率为1、2、4、8、12、32、64KSPS,可调还是说自适应的?
2、在硬件设计时,ADS131e04芯片采样速率如何设置?
3、为了使ADS131e04芯片采样速率和C6748匹配,C6748的时钟如何考虑?
Titan:
例程SPIFlash的SetUpSPI函数中,SPIclkConfigure(SOC_SPI_1_REGS,150000000,20000000,SPI_DATA_FORMAT0);
此函数为配置SPI的clk,其中150000000和20000000代表什么?
SPIclkConfigure()函数参数的含义从哪可以获知?
现在我需要用到spi0和spi1两个spi口,请问:可以在SetUpSPI函数中直接对两个SPI口初始化,如下
{
...
...
SPIclkConfigure(SOC_SPI_0_REGS,150000000,20000000,SPI_DATA_FORMAT0);
SPIclkConfigure(SOC_SPI_1_REGS,150000000,20000000,SPI_DATA_FORMAT0);
...
...
}
上述方法是否正确?spi0和spi1会冲突吗?