This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6678EVM 使用STK例程下载的一个小问题- memory address问题



硬件: 6678 EVM 

软件: CCS 6.1 ; 安装 bios_mcsdk_02_01_02_06_setupwin32

问题:

使用STK GPIO的例子,通过编译,有warning 如下

板子进行连接  test connection一切正常,但是下载的时候,出现问题。。貌似是内存地址什么问题。。求指点! 

我觉的可能和cmd文件有关系,但是这个是自带的,现贴出

-heap  0x800
-stack 0x1000

MEMORY
{
	/* Local L2, 1MB*/
	VECTORS: 	o = 0x00800000  l = 0x00000200   
	LL2_RW_DATA: 	o = 0x00800200  l = 0x5FE00   

	/* Shared L2 2MB*/
	SL2: 		o = 0x0C000000  l = 0x00200000   
	
	/* External DDR3, upto 2GB per core */
	DDR3_CODE: 	o = 0x80000000  l = 0x01000000   /*set memory protection attribitue as execution only*/
	DDR3_R_DATA: 	o = 0x81000000  l = 0x01000000 	 /*set memory protection attribitue as read only*/
	DDR3_RW_DATA: 	o = 0x82000000  l = 0x06000000   /*set memory protection attribitue as read/write*/
}

SECTIONS
{
	vecs       	>    VECTORS 

	.text           >    LL2_RW_DATA
	.cinit          >    LL2_RW_DATA
	.const          >    LL2_RW_DATA
	.switch         >    LL2_RW_DATA

	.stack          >    LL2_RW_DATA
	GROUP
	{
		.neardata
		.rodata
		.bss
	} 		>    LL2_RW_DATA
	.far            >    LL2_RW_DATA
	.fardata        >    LL2_RW_DATA
	.cio            >    LL2_RW_DATA
	.sysmem         >    LL2_RW_DATA
}

在线等~谢谢