This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教关于CCS5.4 C6670 EDMA3 二维搬移最大长度



各位专家好!

         在CCS5.4 下调试EDMA3时遇到一个问题,使用demo edma3_drv_bios6_c6678be_st_sample 进行AB模式(二维)下搬移,发现不能达到一次最大传输65535*65535字节长度。具体如下:

  一维EDMA搬移时,一次EDMA可以最大搬移65535B,是没有问题的;

2.  在进行二维AB搬移时,我们理解是一次最大可以搬移 65535 * 65535 * 65535个字节,但是实际测试时发现

 Acnt* bcnt 不能超出65535B,超出部分搬移不过去。

 不知道这个与什么有关,请各位专家帮忙分析下,多谢!

 

代码如下:

************************

 

EDMA3_DRV_Result edma3_test(
                                    EDMA3_DRV_Handle hEdma,
                                    unsigned int acnt,
                                    unsigned int bcnt,
                                    unsigned int ccnt,
                                    EDMA3_DRV_SyncType syncType)
    {
    EDMA3_DRV_Result result = EDMA3_DRV_SOK;
    EDMA3_DRV_PaRAMRegs paramSet = {0,0,0,0,0,0,0,0,0,0,0,0};
    unsigned int chId = 0;
    unsigned int tcc = 0;
    int i;
    unsigned int count;
    unsigned int Istestpassed = 0u;
    unsigned int numenabled = 0;
    unsigned int BRCnt = 0;
    int srcbidx = 0, desbidx = 0;
    int srccidx = 0, descidx = 0;

    acnt=65535;
    bcnt=2;
    //srcBuff1 = (signed char*) GLOBAL_ADDR(_srcBuff1);
    //dstBuff1 = (signed char*) GLOBAL_ADDR(_dstBuff1);

    srcBuff1 = (unsigned char*) 0xE1000000;//GLOBAL_ADDR(_srcBuff1);
    dstBuff1 = (unsigned char*) 0xE2000000;//0x4001FC80;//GLOBAL_ADDR(_dstBuff1);


    /* Initalize source and destination buffers */
    for (count = 0u; count < (acnt*bcnt*ccnt); count++)
        {
       *((unsigned char*)0x00880000 + count) = (int)count;
        /**
         * No need to initialize the destination buffer as it is being invalidated.
        dstBuff1[count] = initval;
        */
        }

 

    /*
    * Note: These functions are required if the buffer is in DDR.
    * For other cases, where buffer is NOT in DDR, user
    * may or may not require the below functions.
    */
    /* Flush the Source Buffer */
    if (result == EDMA3_DRV_SOK)
        {
        result = Edma3_CacheFlush((unsigned int)srcBuff1, (acnt*bcnt*ccnt));
        }

    /* Invalidate the Destination Buffer */
    if (result == EDMA3_DRV_SOK)
        {
        result = Edma3_CacheInvalidate((unsigned int)dstBuff1, (acnt*bcnt*ccnt));
        }
/* EDMA3_ENABLE_DCACHE */


    /* Set B count reload as B count. */
    BRCnt = bcnt;

    /* Setting up the SRC/DES Index */
    srcbidx = (int)acnt;
    desbidx = (int)acnt;
    if (syncType == EDMA3_DRV_SYNC_A)
        {
        /* A Sync Transfer Mode */
        srccidx = (int)acnt;
        descidx = (int)acnt;
        }
    else
        {
        /* AB Sync Transfer Mode */
        srccidx = ((int)acnt * (int)bcnt);
        descidx = ((int)acnt * (int)bcnt);
        }


    /* Setup for Channel 1*/
    tcc = EDMA3_DRV_TCC_ANY;
    chId = EDMA3_DRV_DMA_CHANNEL_ANY;

    /* Request any DMA channel and any TCC */
    if (result == EDMA3_DRV_SOK)
        {
        result = EDMA3_DRV_requestChannel (hEdma, &chId, &tcc,
                                        (EDMA3_RM_EventQueue)0,
                                            &callback1, NULL);
        }

    if (result == EDMA3_DRV_SOK)
        {
        /* Fill the PaRAM Set with transfer specific information */
        paramSet.srcAddr    = (unsigned int)(srcBuff1);
        paramSet.destAddr   = (unsigned int)(dstBuff1);

        /**
         * Be Careful !!!
         * Valid values for SRCBIDX/DSTBIDX are between �2768 and 32767
         * Valid values for SRCCIDX/DSTCIDX are between �2768 and 32767
         */
        paramSet.srcBIdx    = srcbidx;
        paramSet.destBIdx   = desbidx;
        paramSet.srcCIdx    = srccidx;
        paramSet.destCIdx   = descidx;

        /**
         * Be Careful !!!
         * Valid values for ACNT/BCNT/CCNT are between 0 and 65535.
         * ACNT/BCNT/CCNT must be greater than or equal to 1.
         * Maximum number of bytes in an array (ACNT) is 65535 bytes
         * Maximum number of arrays in a frame (BCNT) is 65535
         * Maximum number of frames in a block (CCNT) is 65535
         */
        paramSet.aCnt       = acnt;
        paramSet.bCnt       = bcnt;
        paramSet.cCnt       = ccnt;

        /* For AB-synchronized transfers, BCNTRLD is not used. */
        paramSet.bCntReload = BRCnt;

        paramSet.linkAddr   = 0xFFFFu;

        /* Src & Dest are in INCR modes */
        paramSet.opt &= 0xFFFFFFFCu;
        /* Program the TCC */
        paramSet.opt |= ((tcc << OPT_TCC_SHIFT) & OPT_TCC_MASK);

        /* Enable Intermediate & Final transfer completion interrupt */
        paramSet.opt |= (1 << OPT_ITCINTEN_SHIFT);
        paramSet.opt |= (1 << OPT_TCINTEN_SHIFT);

        if (syncType == EDMA3_DRV_SYNC_A)
            {
            paramSet.opt &= 0xFFFFFFFBu;
            }
        else
            {
            /* AB Sync Transfer Mode */
            paramSet.opt |= (1 << OPT_SYNCDIM_SHIFT);
            }

        /* Now, write the PaRAM Set. */
        result = EDMA3_DRV_setPaRAM(hEdma, chId, &paramSet);
        }


    /*
     * There is another way to program the PaRAM Set using specific APIs
     * for different PaRAM set entries. It gives user more control and easier
     * to use interface. User can use any of the methods.
     * Below is the alternative way to program the PaRAM Set.
     */

    /*
    if (result == EDMA3_DRV_SOK)
        {
        result = EDMA3_DRV_setSrcParams (hEdma, chId, (unsigned int)(srcBuff1),
                                        EDMA3_DRV_ADDR_MODE_INCR,
                                        EDMA3_DRV_W8BIT);
        }

    if (result == EDMA3_DRV_SOK)
        {
        result = EDMA3_DRV_setDestParams (hEdma, chId, (unsigned int)(dstBuff1),
                                            EDMA3_DRV_ADDR_MODE_INCR,
                                            EDMA3_DRV_W8BIT);
        }

    if (result == EDMA3_DRV_SOK)
        {
        result = EDMA3_DRV_setSrcIndex (hEdma, chId, srcbidx, srccidx);
        }

    if (result == EDMA3_DRV_SOK)
        {
        result =  EDMA3_DRV_setDestIndex (hEdma, chId, desbidx, descidx);
        }

    if (result == EDMA3_DRV_SOK)
        {
        if (syncType == EDMA3_DRV_SYNC_A)
            {
            result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt,
                                                BRCnt, EDMA3_DRV_SYNC_A);
            }
        else
            {
            result = EDMA3_DRV_setTransferParams (hEdma, chId, acnt, bcnt, ccnt,
                                                BRCnt, EDMA3_DRV_SYNC_AB);
            }
        }

    if (result == EDMA3_DRV_SOK)
        {
        result = EDMA3_DRV_setOptField (hEdma, chId,
                                        EDMA3_DRV_OPT_FIELD_TCINTEN, 1u);
        }

    if (result == EDMA3_DRV_SOK)
        {
        result = EDMA3_DRV_setOptField (hEdma, chId,
                                        EDMA3_DRV_OPT_FIELD_ITCINTEN, 1u);
        }

    */


    /*
     * Since the transfer is going to happen in Manual mode of EDMA3
     * operation, we have to 'Enable the Transfer' multiple times.
     * Number of times depends upon the Mode (A/AB Sync)
     * and the different counts.
     */
    if (result == EDMA3_DRV_SOK)
        {
        /*Need to activate next param*/
        if (syncType == EDMA3_DRV_SYNC_A)
            {
            numenabled = bcnt * ccnt;
            }
        else
            {
            /* AB Sync Transfer Mode */
            numenabled = ccnt;
            }

        for (i = 0; i < numenabled; i++)
            {
            irqRaised1 = 0;

            /*
             * Now enable the transfer as many times as calculated above.
             */
            result = EDMA3_DRV_enableTransfer (hEdma, chId,
                                                EDMA3_DRV_TRIG_MODE_MANUAL);
            if (result != EDMA3_DRV_SOK)
                {
                printf ("edma3_test: EDMA3_DRV_enableTransfer " \
                                    "Failed, error code: %d\r\n", result);
                break;
                }

            /* Wait for the Completion ISR. */
            while (irqRaised1 == 0u)
                {
                /* Wait for the Completion ISR. */
                printf ("waiting for interrupt...\n"); 
                }

... ....